STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB port on 32L152CDISCOVERY

Posted on October 22, 2014 at 09:16Hi, I notice that the 32L152CDISCOVERY device has only1 USB port, which is connected to the ST-LINK V2 part. Can I configure this port for ''user'' USB communication as part of my application running on the STM32L1...

bnp979 by Associate III
  • 1525 Views
  • 3 replies
  • 0 kudos

usb bootloader in cortex-m3

Posted on October 16, 2014 at 12:50Hi everybody, this is my first post on STe2e, so be patient with me. I've read a good amount of threads related to bootloaders/interrupt/VTOR but I cannot find a final word to my problem so I decided to start a new...

STM32F0 UART not sending data

Posted on October 20, 2014 at 11:20 I'm new in ST world. I'm trying to work with UART, so I wrote this code to initializate UART and to send ''Hello''. I'am using STM32F0 board. #include ''stm32f0xx_gpio.h'' #include ''stm32f0xx_rcc.h...

mahfoudhi by Associate II
  • 2370 Views
  • 4 replies
  • 0 kudos

What is the best IDE for STM32?

Posted on October 22, 2014 at 09:51used for many yearsKeilproducts,butlatelyI findthat it containsmore errors,backlogsandproblems thanis healthy.Is thereTrueStudioorIAREmbeddedWorkbenchforARMbetter?

asrock70 by Associate II
  • 2569 Views
  • 7 replies
  • 0 kudos

Virtual Com example in Iar 6.50

Posted on October 22, 2014 at 17:33Hi guys,after the Iar Embedded Workbench 6.50 installation, I found this folder in this path:...\ST\arm\examples\ST\STM32L1xx\IAR-STM32L152VB-SK\VirtualComCan someone explain me how can I use this example on my stm...

ndonj86 by Associate II
  • 1080 Views
  • 1 replies
  • 0 kudos

stm32f429 and sdram

Posted on July 11, 2014 at 17:58hello every onei use stm32f429 disco and keil compileri need to load a .bmp file to sdramthe .bmp file is about 230400 bytesso i define DATA_IN_ExtSDRAM and i config the options like attached filebut it makes hard fau...

STM32F3 DMA and concurrent memory access

Posted on October 22, 2014 at 11:00Hello, I'm new in STM32 World. I have a question:I enable ADCs in my STM32F3 with dma access and microcontroller works very well, but, in F3 is not possible double buffering or pinpong method with dma, correct?So, ...

lrosadev by Associate II
  • 1072 Views
  • 1 replies
  • 0 kudos

BSDL files for STM32F373

Posted on October 22, 2014 at 11:51I have tried to locate a BSDL file for STM32F373VCT6 ? anywhere to be found?//Pierre

ekapiwi by Associate
  • 955 Views
  • 1 replies
  • 0 kudos

HAL_SPI_TransmitReceive_IT() never completes

Posted on October 20, 2014 at 13:10I am having an issue with the STM32Cube HAL function, HAL_SPI_TransmitReceive_IT(). I am using the STM32CubeF2 library with STM32CubeMX tool to generage most of the initialisation code.I have an STM3220G evalutatio...

andrew by Associate II
  • 3361 Views
  • 5 replies
  • 0 kudos

RDP and PCROP spurious activation

Posted on October 22, 2014 at 09:52 Hi, I have a flash init routine that I call after enabling the main PLL in my boot loader and my main application. The routine will check in the bootloader if the OPTCR or OPTCR1 values have been changed fo...

mfm by Associate II
  • 2317 Views
  • 4 replies
  • 0 kudos