STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC calibration on sTM32f3 discovery

Posted on February 21, 2013 at 15:46I meet difficulties to understand the RTC calibration protocoles presented in the UM1581, the RM0316 or the AN3371.Two distincts calibration procedures are discussed there in :- a coarse one, - a smooth one. For w...

STM32F429 FMC SDRAM problem

Posted on April 22, 2014 at 08:37Hi, I am using STM32F429ZIT6 in my new design. I got a Rev.Y silicon from DIGIKEY. I found that the SDRAM cannot be used as stack or heap, and now I know there is a problem as stated ES0206 “2.8.7 FMC dynamic and sta...

jasonj2 by Associate II
  • 1577 Views
  • 2 replies
  • 0 kudos

Changing STM32 sysclk in run mode

Posted on October 23, 2014 at 19:20Good day,Is it possible to change system clock (PLL) during run mode.I tried to change it with this one, but does not worked:RCC->PLLCFGR = PLL_M | (PLL_N << 6) | (((PLL_P >> 1) -1) << 16) |                   (RCC_...

hitsumen by Associate II
  • 1477 Views
  • 2 replies
  • 0 kudos

STM32F407 Placing all code in RAM

Posted on October 23, 2014 at 21:17  The original post was too long to process during our migration. Please click on the attachment to read the original post.

saulr by Associate II
  • 3653 Views
  • 6 replies
  • 0 kudos

STM32F429I-DISCO and XTAL X3 8MHz

Posted on October 21, 2014 at 23:30 Hi, Its my first time here! I have a STM32F429I-DISCO, original from factory. I used the STM32CubeMX with STM32Cube_FW_F4_V1.3.0 to build a code. I selected ''new project\board selector\...

ricardodm by Associate II
  • 3055 Views
  • 9 replies
  • 0 kudos

Measuring a time between two events with SysTick on STM32F4?

Posted on October 23, 2014 at 20:45Hello all, i want to build a function like current_time = time_now - last_time,  more exactly i wanna  get the time from two of the same event (reading some mems sensors) I'ved google`it a bit and found that most u...

Bogdan by Senior
  • 3038 Views
  • 3 replies
  • 0 kudos

stm32f030 jtag connection

Posted on May 02, 2014 at 06:46 hi, i am very new to stm32,i have to make jtag connection also for debugging and programming. i have concerned with stm32f030R8t6 disco schematic but i was unable to find more detail about 20pin jtag as its using st_l...

How do I connect the STM32F4 Discovery to external power?

Posted on October 22, 2014 at 07:20For the STM32F4 Discovery board, can someone tell me exactly what pins need to be connected in order to power this externally (i.e. not via USB)? Surprisinginly, I can't find any place where this information is cle...

sandtime by Associate II
  • 5258 Views
  • 3 replies
  • 0 kudos

STM32F429I-DISCO 2.4'' LCD Problem (white lcd)

Posted on October 02, 2014 at 14:29Hello all. I have a discovery board with the 2.4'' LCD.When i download any example with GUI in all situations and wait some time the screen goes white.  Does anyone knows why and if the board is defective.Thanks.

0690X00000602yHQAQ.jpg 0690X00000602yMQAQ.jpg
issaiass by Associate
  • 1222 Views
  • 2 replies
  • 0 kudos