STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L152VC: LCD segments not all 5V tolerant

Posted on October 21, 2014 at 19:36The STM32L152VC includes an internal voltage regulator with contrast control from 2.60 to 3.51V. Those voltages then get used to drive the individual segments. In my case, I'm running the processor at 2.6V (VD). Wh...

sheldon by Associate II
  • 1069 Views
  • 1 replies
  • 0 kudos

Hard fault error and static variable

Posted on October 15, 2014 at 10:14Hello all, Following some hardfault error with my code running into a STM32F415, I found a solution that leave me puzzled. In my main, I declare a array of 600 uint8_t called data;uint8_t data[600]; I call a funct...

ARM GCC + STM32 don't like each other

Posted on October 16, 2014 at 16:29Hello matesI'm looking to use the SMT32F303VC (STM32F Discovery Board) for my first product. I'm developing on mac osx, build my toolchain based on ARM GNU GCC (GCC ARME NONE EABI 4.8) + Eclipse + Zylin Plugin + Op...

STM32F4 Discovery slow speed

Posted on October 21, 2014 at 00:00 Hi all, I am working with the STM32F4 Discovery board and I changed the Standard Periph Library from 1.0 to 1.4 With the 1.4 version the boards run slow with this code: #include ''stm32f4xx_c...

danelifab by Associate II
  • 1815 Views
  • 4 replies
  • 0 kudos

Sending ten bits to SPI slave

Posted on October 18, 2014 at 20:19Hi, I want to send ten bits from my STM32F4 Discovery to a SPI slave. The SPI Init struct only allows 8- or 16 bit (SPI_DataSize_8b, SPI_DataSize_16b) Whats the best way to send the required ten bits to the SPI sla...

paul2 by Senior
  • 1187 Views
  • 3 replies
  • 0 kudos

STM32-Disco429 SDIO + SD CARD init

Posted on September 20, 2014 at 04:23HelloMicro controller = STMF32DISCO429.SD card reader = SD/MMC CARD BREAKOUT BOB-12941SD CARD = 16mb Hp invent Sandisk card 0210ln Library = STM32Cube_FW_F4_V1.3.0Hello, ive been trying to set up a sd card just s...

s3322513 by Associate
  • 1157 Views
  • 1 replies
  • 0 kudos

OpenOCD or AttolicGDB flash error with STM32F030 (F05x ok)

Posted on September 24, 2014 at 09:37We have good experience with STM32f100, STM32F05x but for our new product we used STM32F030 and I am not able to program it over GDB. The interesting think is that F05x can be programmed over GDB without errors (...

hub by Associate II
  • 2121 Views
  • 3 replies
  • 0 kudos

stm32f051 - st8034 reader switching

Posted on October 21, 2014 at 15:14Hello all ,            Can any one help me how to switch two smart card readers ST8034hc with one MCU - STM32F051XX . Please provide me with some example file or application note , schematic files   with smart card...

sarat by Associate
  • 643 Views
  • 0 replies
  • 0 kudos

STM32F303xC Starting one timer with another timer UE

Posted on October 21, 2014 at 14:19Hello everyone, i am trying to start another timer with another timer update event. I tried to follow RM(see picture attached) and it seems that i did everything as it states, but maybe i understand something wrong...

STM32F2xx VCP Open Port Failed

Posted on October 20, 2014 at 07:48I am using STM32F2xx and I emulate it as a VCP driver, I used the sample code from STM32 for the USB device exampleI wrote a .NET application to open the serial port communication, but I have problem to open the po...

ho by Associate II
  • 5056 Views
  • 11 replies
  • 0 kudos