STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX MDK-ARMV5 project generation problem

Posted on April 08, 2015 at 14:50Hi,I have a problem with MDK-ARMV5 project generation if the project is located on a network drive. Everything else is generated.If I have the project on a local disk everything works OK. I know that this is a simple...

blaz2 by Associate
  • 1665 Views
  • 3 replies
  • 0 kudos

Is my stm32f103 chip's execution speed too slow?

Posted on April 15, 2015 at 18:02Hi,    I have several time strict  TIMER ISR and I tested the execution time of one of them.The result is that 47 instructions(indluding 3 branch instructions) costs 3 us.My chip is stm32f103 and all code and data is...

360804365 by Associate II
  • 1818 Views
  • 5 replies
  • 0 kudos

ADC using DMA

Posted on April 10, 2015 at 12:25I'm using a stm32f429 running at 144MHz and I wanted to implement a periodic two-channel adc conversion. I need to make the conversions on a 1us period and I'm considering in using a dma adc conversion. I know how to...

damasosb by Associate II
  • 1724 Views
  • 3 replies
  • 0 kudos

needing low speed SPI communication

Posted on April 12, 2015 at 16:50Hello everyone! I am using STM32F103RET for my project. I need to communicate by SPI with a low speed digital device with the speed of at most 1KHz clock. At the same time, I need to have my own cpu clock as high as ...

abbas by Associate II
  • 1690 Views
  • 4 replies
  • 0 kudos

Power down reset feature to back up the external SRAM data

Posted on April 14, 2015 at 15:33Hi,I want to use external SRAM with the controller STM32F429. i want to make use of internal supervisor circuit, which is used to power the internal RTC and internal 4Kb SRAM, to backup the data in external SRAM. for...

vini by Associate II
  • 1435 Views
  • 2 replies
  • 0 kudos

Volatile uint8_t variable in interrupts

Posted on April 14, 2015 at 21:51 Hello, I have function fifo_read(RxFifo, &rx, 1) which reads byte from FIFO buffer. I want to use this function in two different interrupt handlers. I have declared rx variable as fo...

hospodar by Associate III
  • 2570 Views
  • 2 replies
  • 0 kudos

Debugger: Could not stop Cortex-M device

Posted on April 14, 2015 at 23:01I've made several custom STM32F4 boards.Never any problems, until now, when my JLINK detects my board ONLY, if I press reset button before I press detect device in Keil uVision.When I press download button I got erro...

tm3341 by Associate II
  • 1341 Views
  • 0 replies
  • 0 kudos