User Activity

Greetings. I am sharing a SPI bus between a H3LIS100DL, a IIS2DLP and an external flash chip. When communicating with external flash, I get corrupted bytes after certain byte sequences. I’ve chased the issue down to the fact that these two accelerome...
Greetings. I am familiar with the general sleep-to-wake functionality, I've used it successfully in the IIS2DH. However I am having issues with the H3LIS100DL. I believe I've enabled sleep-to-wake using control register 5, I've configured the interru...
Posted on February 19, 2016 at 17:26Greetings. I would like to use the LPS25H/B as a pressure measuring device up to ~15 psi ''differential''. I know that the datasheet lists the functional range from 260 to 1260hPa absolute, how does this translate...
Posted on September 26, 2014 at 14:47Greetings. I am trying to determine the best methodology to capture an input pulse train (from a motor encoder), compare the input count to a set point, and generate an event when the input count reaches the setp...