STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F072CBT6 Reset

Posted on April 17, 2015 at 10:48Hi thereI designed a print with a STM32F072CBT6 and connect with a Discovery Board.First I designed the software on the Discovery Board. After that, i want to test the connection to the CBT6. My Code works fine on th...

pfischer by Associate
  • 821 Views
  • 0 replies
  • 0 kudos

RM0090 published uart baud rates

Posted on April 14, 2015 at 06:06Hello, I have a stm32f429 discovery board. I am trying to confirm that I can achieve the max baud rates listed in the RM0090 document. I have tried using a pclk of 42 and 84 mhz, with oversampling of 8x and 16x. The ...

renasis by Associate II
  • 2978 Views
  • 8 replies
  • 0 kudos

My own BOOTLOADER with STM32F0

Posted on April 16, 2015 at 15:59Hi!  I'm  using MTF32F030R8 and I need to   develope  my own bootloader.  I use the first 8K of flash for bootloader (from 0x800000 to 0x8001FFF) and from 0x8002000 my SW  application. I'm not finding how to set the ...

lisa by Associate
  • 1378 Views
  • 4 replies
  • 0 kudos

PWM Input Capture via CH3 and CH4

Posted on April 16, 2015 at 14:12Hello I want to measure the duty cycle of an input frequency on the stm32f4. For that I need to use the TIM3 or TIM8 and there I have to use channel CH3 and CH4. But now I'm looking for TIM_PWMIConfig(...) and there ...

oli by Associate II
  • 3544 Views
  • 6 replies
  • 0 kudos

Boot1

Posted on April 13, 2015 at 16:50Where is the boot1 pin on STM32F3? More specifically STM32F334?

adaniel by Associate III
  • 1062 Views
  • 2 replies
  • 0 kudos

Power up STM32F407 Discovery using a 11.1V Battery

Posted on April 16, 2015 at 10:56Hello STM32-Community!I read in the document UM1472 that the 5V pin can be used as a input of an external power supply. I want to power up my board by using one battery (11.1V). I was thinking about a simple voltage ...

0690X00000605ZUQAY.png
yannick2 by Associate
  • 1179 Views
  • 1 replies
  • 0 kudos

STM32F4 8bit DMA to GPIO

Posted on April 16, 2015 at 17:05 Hello, I'm relatively new to the STM32F4 family but have worked with other microcontrollers in the the past. I'm trying to use DMA to send 8bits of data at a time from a memory array to a GPIO (GPIO_C) using ...

borisw37 by Associate
  • 1586 Views
  • 1 replies
  • 0 kudos

ST-LINK_CLI Board Serial Number

Posted on March 17, 2015 at 18:40Hi, I have multiple STM32F4 discovery boards connected to the same pc. I use the ST-LINK_CLI utility to burn my user applications and reset them. Is there any way I can have access to the SN field that the ST-LINK_CL...