User Activity

Hello, i try to configure a STM32H7S7L8H6H in CubeMX and it seems that, when Ethernet RMII is configured, SDMMC2 is unusable because there are some pins like PC1 which can't be remapped. Can this be true?This chip is designed for external memories an...
Hi, i have a custom board with a STM32 and a Touchscreen.The TSC is connected via I2C to the STM32.There are other I2C slave devices connected to this I2C bus, as well.And i have two threads, a system thread and a gui thread (where Touch GFX is runni...
Hello,i use at a STM32F429 the PD5 pin to drive a PNP BJT transistor to switch a sensor supply:PD5 is configured as open drain, and when the stm32 is pulling PD5 low, the transistor supplies the sensor with 5V power. This works so far.But when PD5 is...
Hello,when i click on a .ioc file within CubeIDE, CubeMX is opened inside of CubeIDE. It starts opening the ioc file and shows progress bars: But then, after opening, it shows only a tab with no content.Does someone know whats wrong here? I use:Debia...
Hello, When i configure a project with CubeMX and TouchGFX Generator stuff and save this,after a new start of CubeMX and opening the .ioc file again i get this error message:And my TouchGFX Generator Configuration is lost. The other configuration is ...