STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Connecting two STM32F4s with HC-05 Bluetooth

Posted on April 29, 2015 at 19:20I connected HC-05 to my STM32F4 through USART. I have tested it with android app, and everything seems to work good (sending, receiving data). But how to connect two STM32F4s with each other? Do I have to know addres...

Bug in STM32CubeMX - maximum ADC clock

Posted on October 30, 2014 at 10:35Not sure if this is a bug or just a missing feature, but I'll explain what I'm doing!I am using STM32CubeMX version 4.3.0 to configure clocks on an STM32F407IEHx.When setting values in the clock configuration, cloc...

iguffick2 by Associate III
  • 1180 Views
  • 2 replies
  • 0 kudos

STM32F105 Dual CAN Filters

Posted on April 24, 2015 at 12:18On this processor both bxCAN cells share the filters located in CAN1. There is only a single CAN_FFA1R register whose bits are used to assign individual filters to FIFO 0 or FIFO 1. There is no bit allocating them to...

STM32F103 Clock Configuration

Posted on April 28, 2015 at 23:47Hi,I have a question concerning the clock configuration of an STM32F103RBT6. I used several STM32F4 chips before and generated the system_stm32f4xx.c file with the STM32F4 Clock Configuration Tool. It seems that ther...

ST7570 ST7580 C Library

Posted on June 22, 2011 at 10:17 Where can I get the C Library for the powerline trancievers ST7570 and ST7580 described in User Manual UM1070? http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/DM00026249.pdf The...

dgeoerg9 by Associate
  • 1842 Views
  • 3 replies
  • 0 kudos

STM32CubeMX: SDIO 4bit issue

Posted on April 15, 2015 at 17:33STM32F429 Generated Code does not initialize all pins correctly, some should be set to open drain highspeed, this has to be done manually. Without this only 1bit mode works correctly 4bit gets stuck. We use a 2GByte ...

Quadrature encoder simulation

Posted on April 28, 2015 at 16:49Hello I am using the STM32F4 interfaced with two hall effect quadrature encoders.Is there a method to generate the signals (A,B) coming from the encoder to validate my work ? because now i don't have the sensor  #...

Cesar cfg by Associate II
  • 1922 Views
  • 5 replies
  • 0 kudos

Where is the datasheet? OR Where is my tutorial?

Posted on April 29, 2015 at 14:24I bought a discovery board with STM32F4 family processor (comes with a TFT LCD). I have my IDE working and downloaded CubeMX and generated some init code - no problem.Now, I don't know how to do anything! How do I to...