STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4xx system clk

Posted on April 29, 2015 at 10:46Hi,I have a doubt concerning the clock architecture of the MCU in subject.Can the System Clock be used directly for any master (CPU core, DMA etc.) without passing through the AHBx prescaler. The reason for this ques...

damiano2 by Associate
  • 1160 Views
  • 3 replies
  • 0 kudos

How to init GPIO on CubeMX generated code ?

Posted on April 26, 2015 at 11:42 Guys, I have generated a code for Keil from CubeMx but I can't initialize GPIO, I can see a code in main.c below....anyone knows how to initialize GPIO,reset and set a bit on it at CubeMx generated c...

Timeout error trying to connect via ''external mode''

Posted on April 01, 2015 at 19:10Hi, I posted a question yesterday which was solved by myself about the external mode connection. But now I am getting another problem, a timeout error. I am using the ''Embedded Coder Support Package for STMicroelect...

GPIOE and ETH on STM32F107

Posted on April 28, 2015 at 14:51Guys, Is GPIOE related with ETH on STM32F107 ? I tried to activate ETH and I can't send command to GPIOE ?? Are the multiplexed together ? Any clues ? thanks #i-have-a-clue

stm32F0

Posted on April 28, 2014 at 08:07Hi,I developed my project with stm32F0discovery and is OK. Now, I load my project to our board (final product) and I have a problem with timers and systick. For example: tim14 is set to operate 1 msec, instead I see ...

mosine by Associate II
  • 1622 Views
  • 6 replies
  • 0 kudos

stm32f103 encoder mode with as5040

Posted on April 26, 2015 at 22:50 Hi, I have problem with encoder mode. AS5040 is in quadrature output. I use this code and it doesnt work, where is the problem? void gpio_conf(void) { GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2Peri...

ov7670 clock supply

Posted on April 23, 2015 at 12:07HelloIs it sufficient to supply ov7670 camera module xclk pin with MCO1/2 pins of stm32f4? 

STM32F030 input protection diodes

Posted on April 28, 2015 at 13:29Hello!I've been reading through the reference manual of the F030 and noticed the structure of the GPIOs ... I've noticed they don't have any input protection diodes. The F100 and others have two clamping diodes on 3....

tomaz by Associate
  • 1024 Views
  • 1 replies
  • 0 kudos