STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_RTC_SetTime Timeout

Posted on June 22, 2015 at 11:33Hello,HAL_RTC_SetTime fails when trying to set new values on the RTC due to RTC_EnterInitMode timeout.while((hrtc->Instance->ISR & RTC_ISR_INITF) == (uint32_t)RESET){ if((HAL_GetTick() - tickstart) >  RTC_TIMEOUT_VALU...

George.P by Associate III
  • 1415 Views
  • 1 replies
  • 1 kudos

SDIO small buffer write speed

Posted on June 20, 2015 at 09:10Good day,I have a bit of a problem, is it possible to use SDIO with smaller buffers and have decent speed.I tried to do few tests with smaller buffer like data_buffer[512], data_buffer[1024]...And have really poor spe...

hitsumen by Associate II
  • 884 Views
  • 2 replies
  • 0 kudos

STM32F373 USART2 Problem

Posted on May 11, 2015 at 13:14Hello, I have some problem with USART2 (stm32f373). USART1 is working with same code but, Usart2 does not work.  here is the code. void Uart_Int(void) {   GPIO_InitTypeDef GPIO_InitStructure;   USART_InitTypeDef USART_...

fslhusni by Associate II
  • 2937 Views
  • 7 replies
  • 0 kudos

STM32F4RGT6 random initialization issue

Posted on June 21, 2015 at 14:51Hello again!We have designed the board with this processor, it works perfectly.But in 1 : 100 times it seems as there is some weird condition and the processor wont initialize at all.If this situation happen, then I c...

zexx86 by Associate II
  • 1970 Views
  • 2 replies
  • 0 kudos

STM32F4 SPI - RXNE never gets asserted.

Posted on June 20, 2015 at 20:02Hi,I am debugging the SPI interface on the STM32F427 for a while now. I am using SPI1 and SPI2. SPI1 works just fine, I am able to transmit and receive data just fine. Now I am struggling to get SPI2 to work fully.I c...

STM32 bootloader USART1 only

Posted on June 19, 2015 at 18:25Hello,I have encountered issue when using STM32 bootloader, because by default it seems that it scanning all USARTs.Unfortunately I have to use only USART1, because other USARTs are used for other purposes and can tra...

zexx86 by Associate II
  • 2802 Views
  • 6 replies
  • 0 kudos

STM32F103x8: What's the correct command-line define ?

Posted on June 20, 2015 at 04:05I have a STM32F103c8 device and am trying to use STM32F1Cube with it.But if I use the -DSTM32F103x8=1 define on my gcc command-line, I get the following error:Please select first the target STM32F1xx device used in yo...

pacman by Associate III
  • 1361 Views
  • 1 replies
  • 0 kudos

STM32F0 USART notworking

Posted on November 07, 2014 at 06:37 Hi, I am trying to some data from STM32FO devboard(Standard board from ST- MB1304) to PC via usart1. I have created the project in Keil. Data is not transmitting from STM32 to PC. First I thought that cod...

aruns06 by Associate II
  • 2885 Views
  • 6 replies
  • 0 kudos