STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L010RB_NUCLEO_PWR_STANDBY

Hello, I have tested the kit discovery  NUCLEO-L010RB and the program PWR STANDBY(mcu STM32L010RB), this work fine. I would like do exactly the same test with the mcu STM32L010K8 (so the same family like STM32L010RB), but I have a problem, the progra...

Nonotiboy by Associate II
  • 3955 Views
  • 6 replies
  • 1 kudos

Resolved! SPI NSSP on STM32F767ZI

Hello,Disclosure: I am fairly new to using STM based Microcontrollers, as well as DMA.I am using an STM32F767ZI MCU on a custom PCB. I am trying to Implement an SPI interface to an DAC Chip (AD5443) through DMA (no interrupts as of the moment). My DM...

sinannov_1-1733871204901.png
sinannov by Associate II
  • 2745 Views
  • 4 replies
  • 2 kudos

Dual CAN on G491 (bare metal)

Hello,I implemented a FDCAN in bare metal on the STM32G491 that works on FDCAN1 (with one unrelated problem). Now I need the second one too. So when I try to send over FDCAN2 only garbage comes out on the CAN bus. Yet the CRC is correct so it is actu...

Resolved! STM32N6

It's been almost two years since word first appeared about STM32N6, but there is still no public information about when it will actually show up.Can we expect some news about it at the STM32 Summit next week?If not, what can one do in order to get so...

TLin.5 by Associate III
  • 2806 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H723 Input capture timer over DMA using Low Layer

  Hello STM Community,   I want to implement on STM32H723 ultrasonic sensor and I use TIM8 Input Capture mode to read time between falling edges. It worked on interrupts, but I want to use DMA in order prevent interrupt storm and to speed up calcula...

adakPal by Associate III
  • 1628 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H743Zit6 board CAN not working

 #include"STM32H743.h" /* CAN Handle */ FDCAN_HandleTypeDef hfdcan1; /* Function to Initialize CAN Peripheral */ void CAN_Init(void) { /*CAN GPIO Configuration (PB12 as RX, PB13 as TX)*/ GPIO_InitTypeDef GPIO_InitStruct = {0}; __HAL_RCC_G...

bhargav23 by Associate II
  • 4721 Views
  • 10 replies
  • 3 kudos

Resolved! FDCAN missed RX interrupt on STM32H743

Hi, i need help with a strange behaviour of the FDCAN RX interrupt. I have 2 controllers which communicate with each other over CAN bus (Classic CAN). The first (my problem mcu) sends a command message and the second answers with 3 messages. The prob...

Phil4 by Associate
  • 4424 Views
  • 5 replies
  • 1 kudos