STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cannot set deadtime for HRTIM1 in NUCLEO-G474

Hello,I have the NUCLEO-G474RE kit and am trying out basic exercises such as toggling GPIO pins, setting up timers and generating PWM gating pulses. I got GPIOs and timers working. I got basic complementary PWM working on Channel A with the HRTIM. Bu...

SKI by Associate
  • 1324 Views
  • 2 replies
  • 1 kudos

STM32F746IGT Boot configuration issue?

Hello you guys.I’m having trouble operating the STM32F746 board.I designed an embedded board using the STM32F746 and attempted to control LEDs through CubeIDE. While compilation and program uploading were successful, the LEDs do not function at all.I...

toywars0_0-1733888685456.png toywars0_4-1733889038144.png toywars0_3-1733888959345.png toywars0_6-1733889312495.png
toywars0 by Associate
  • 1263 Views
  • 2 replies
  • 0 kudos

Resolved! ST future ARM Cortex M55/M85 line?

Are there any plans for ST to release an ARM Cortex M55 or (more hopefully for me) an ARM Cortex M85 line?I am extremely interested in their number-crunching and vectorization features, and am very keen to see how they would perform in a real-time au...

etheory by Senior II
  • 16929 Views
  • 7 replies
  • 3 kudos

Resolved! Struggling with CAN Filter

Dear Community,   Once again I am struggling with CAN Filters for extended IDs using CAN2 on a STM32F765. I have the ID 0x010100 and the filter should look like 0xXX0101XX where the X hex should be ignored. One of my early approaches: uint32_t filter...

Anno by Associate II
  • 4474 Views
  • 8 replies
  • 7 kudos

STM32L010RB_NUCLEO_PWR_STANDBY

Hello, I have tested the kit discovery  NUCLEO-L010RB and the program PWR STANDBY(mcu STM32L010RB), this work fine. I would like do exactly the same test with the mcu STM32L010K8 (so the same family like STM32L010RB), but I have a problem, the progra...

Nonotiboy by Associate II
  • 3897 Views
  • 6 replies
  • 1 kudos

Resolved! SPI NSSP on STM32F767ZI

Hello,Disclosure: I am fairly new to using STM based Microcontrollers, as well as DMA.I am using an STM32F767ZI MCU on a custom PCB. I am trying to Implement an SPI interface to an DAC Chip (AD5443) through DMA (no interrupts as of the moment). My DM...

sinannov_1-1733871204901.png
sinannov by Associate II
  • 2712 Views
  • 4 replies
  • 2 kudos

Dual CAN on G491 (bare metal)

Hello,I implemented a FDCAN in bare metal on the STM32G491 that works on FDCAN1 (with one unrelated problem). Now I need the second one too. So when I try to send over FDCAN2 only garbage comes out on the CAN bus. Yet the CRC is correct so it is actu...

Resolved! STM32N6

It's been almost two years since word first appeared about STM32N6, but there is still no public information about when it will actually show up.Can we expect some news about it at the STM32 Summit next week?If not, what can one do in order to get so...

TLin.5 by Associate III
  • 2790 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H723 Input capture timer over DMA using Low Layer

  Hello STM Community,   I want to implement on STM32H723 ultrasonic sensor and I use TIM8 Input Capture mode to read time between falling edges. It worked on interrupts, but I want to use DMA in order prevent interrupt storm and to speed up calcula...

adakPal by Associate III
  • 1615 Views
  • 2 replies
  • 2 kudos