STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STemWin and Unicode

Posted on August 09, 2015 at 12:07Hello forum. I have some questions about STemWin and Unicode. GUI_UC_DispString is really the only function to display Unicode text? Windows and widgets does not support unicode?

jiri by Associate II
  • 1106 Views
  • 1 replies
  • 0 kudos

STM32F334 Tim2 Input Capture Long Interrupt Latency

Posted on August 06, 2015 at 10:52Hi,Was wondering if anyone has any help for me on this.Device: STM32F334R8T6 (on the nucleo)Frequency: 64MHz (double checked outputting the sysclock on MCO), 2 flash wait statesIDE+compiler: SW4STM32 (free eclipse b...

seeking STM32L152 board - how to find it?

Posted on August 10, 2015 at 06:10Hello, I've built a project with the NUCLEO-L152RE.  Now I'm ready to build a prototype, which needs something smaller than the dev. board.  How do people go about finding a STM32L152 board that has a judicious sele...

ehtsai by Associate
  • 1114 Views
  • 2 replies
  • 0 kudos

STM32F103 UART strange behaviour

Posted on August 10, 2015 at 09:25Hello,I am using UART1 for message reception interrupt driven. When the messages wereonly ASCII characters everything worked just fine. But when I changed to binary modeI can see, that some of non ASCII data are com...

STM32L152 no JTAG after wrong page erase

Posted on August 08, 2015 at 10:46Hello, after an (possibly) invalid page erase attemp I can't reach the micro controller via JTAG. Here is the scenario: I have a bootloader (location 0x8000000 to 0x8003FFF). And a firmware (location 0x8004000 and a...

How can i reduce the baudrate with software

Posted on July 29, 2015 at 08:19Hi again :) i am using bluetooth module in my project. My bluetooth module support 1200 bps to 921.6Kbps.However i need first set up 300 bps.Then i need use 600-1200-2400-4800-9600 or 19200 bps .How can i?

STM32F4X CPU halts after CAN Bus connector unplug

Posted on August 09, 2015 at 14:42Hi, I am using CAN bus on STM32F407 using standard peripheral library.When I unplug CAN bus connector, the CPU halts. After reconnecting CAN bus connector, the CPU is still freezing and needs hardware restart. I wan...

h2399 by Associate II
  • 1584 Views
  • 2 replies
  • 0 kudos

STM32F3Discovery ADC_DMA project

Posted on September 19, 2014 at 14:56Good afternoon,I made a project and i set ADC1 in independent mode and DMA1 to read the information from the adc and then write it to the memory. In the Datasheet and in the Reference manual is writen that the AD...

CPU halts on slave I2C bus shut down

Posted on August 09, 2015 at 15:05The original post was too long to process during our migration. Please click on the attachment to read the original post.

h2399 by Associate II
  • 1728 Views
  • 3 replies
  • 0 kudos