cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 TIM2 ARR requires 32-bit access

Dan Hepler
Associate III
Posted on February 05, 2015 at 21:30

Hello, I found some unexpected behaviour with the 32-bit TIM2 module on STM32F4xx devices, and many others.

When accessing the TIM2->ARR (a 32-bit timer) register, 16-bit writes have the following behaviour. If you try writing 0x0987 to TIM2->ARR, it will actually write 0x098709 The high and low half-words have been written with this value.

I found this behaviour using a DMA transfer, but the problem is much more basic and can be reproduced easily single-stepping through some code.

#include ''stm32f4xx.h''

int main(void)

{

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

/* 32-bit writes to TIM2->ARR work fine */

uint32_t *pARR_32 = (uint32_t *)&TIM2->ARR;

*pARR_32 = 0x00000123;

/* 16-bit writes to TIM2->ARR DO NOT WORK AS EXPECTED*/

uint16_t *pARR_16 = (uint16_t *)&TIM2->ARR;

*pARR_16 = 0x0987;

if( TIM2->ARR == 0x09870987 )

{

while(1); // FAILED: High and low half-words are repeated

}

while(1); // Does not make it here

}

As JW posted below (thanks!), this behaviour is both expected and documented. Hope this helps someone else who may not have realized it.

#stm32-tim2

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on February 05, 2015 at 21:36

No, this is an expected and documented behaviour.

RM0383rev.1 2.1.7:

When a 16- or an 8-bit access is performed on an APB register, the access is transformed

into a 32-bit access: the bridge duplicates the 16- or 8-bit data to feed the 32-bit vector.

RM0383rev.1 13.4 TIM2 to TIM5 registers:

The 32-bit peripheral registers have to be written by words (32 bits).

JW

Dan Hepler
Associate III
Posted on February 05, 2015 at 22:21

JW, thanks for the quick response and RM0383 references.  I am updating my original post to help others who run into this behaviour without expecting it.