STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Advantages of using HSE over HSI

Posted on March 30, 2015 at 03:46I'm developing a project in wich main clock accuracy isn't particurlaly important. I do need to measure time acurately, but I can use the RTC with an external 32.768 KHz crystal for that. I was wondering about the po...

andre by Associate
  • 5624 Views
  • 9 replies
  • 0 kudos

GPIO with stm32l0 discovery

Posted on November 02, 2015 at 12:11 Hi everyone, I'm a newbie of embedded programming and this is my first post. I have a STM32L0 Discovery board and wanted to supply electricity to an external circuit. The external circuit ...

nashimoto by Associate II
  • 2129 Views
  • 4 replies
  • 0 kudos

External crystal on STM32F072.

Posted on November 02, 2015 at 17:08I remember from the 1980s that my colleague responsible for the hardware had some trouble getting an oscillator for our MCU to work. But the last decade designing my own hardware, it seemed as if things had improv...

STM32F051 SPI1 Strange behaviour

Posted on November 02, 2015 at 22:52My problem is that i am not able to write to SPI1->DR. I have a LIS2DH accelerometer on SPI1 and i am able to read �Who_Am_I'' register and it returns correct value. However when i try to read any other register v...

Safety integrity level (SIL) and STM32

Posted on October 31, 2015 at 08:21We are looking to make a product which would be SIL (level  2 or 3) compliant. In that product we use STM32F303.I would like to ask if any of you have experience with SIL? Especially with SIL and STM32 micros. Do y...

matic by Associate III
  • 2089 Views
  • 2 replies
  • 0 kudos

Flash @ STM32F429VIT6

Posted on November 02, 2015 at 00:43Hi,I'm using FLASH to store some data. Everything works great when I write in an empty address. When I try to write in a already used memory position, the stored value becomes to zero!I tried erase the sector befo...

gui2 by Associate II
  • 4675 Views
  • 11 replies
  • 0 kudos

STM32F4: Issues with USART1 Configuration

Posted on October 29, 2015 at 23:45 I'm currently experimenting with writing a driver for USART1 at the register level for the STM32F4 Discovery board. I've followed the initialization procedure on page 963 of RM0090; however, when I connect to ...

STM32F107 Ethernet PHY RMII (MICRELL KSZ8081RNG)

Posted on November 02, 2015 at 19:21In my design the STM32F107 is connected to the MICRELL KSZ8081RNG ETH PHY (which operates in RMII v1.2 mode).Using the LwIP i can  transmit ETH packets to the network but cannot receive any data from the net.Can t...

bemiki by Associate
  • 1153 Views
  • 1 replies
  • 0 kudos