STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM Output on STM3210E-EVAL board

Posted on August 27, 2015 at 23:11 I'm trying to setup one of the LEDs on the STM3210E-EVAL board as a PWM output so that I can vary the brightness. I am targeting the red LED, which is on port F, pin 8. I have setup timer 13 which should be tie...

stm32f4 Help with CAN_ErrorCallback

Posted on October 10, 2015 at 20:29Hello.I have some problem and I can't do anything with it. So, I have CAN bus with two CAN. uP is stm32f407. When is normal work i send data by HAL_CAN_Transmit(&hcan2,5), and  HAL_CAN_Transmit(&hcan1,5). I receive...

[STM32F7 Discovery] - LTDC

Posted on October 30, 2015 at 20:28  The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F030C6T6 ADC reference voltage

Posted on October 26, 2015 at 11:37Hello, I've been going through this STM models datasheet, but I could find info if it is possible, to use the provided Vrefint as ADC reference? In the datasheets I could only find that the ADC reference is Vdd, bu...

matas by Associate II
  • 1370 Views
  • 2 replies
  • 0 kudos

STM32F0 interesting malfunction

Posted on October 30, 2015 at 10:59Hello, I am working on STM32F030C6 it is measuring ADC and sending data through the USART. Everything is good in debug mode until I let it run without break points :D I added pictures how the variables look before ...

matas by Associate II
  • 2357 Views
  • 2 replies
  • 0 kudos

STM32 F429 Discovery ADC DMA example very slow

Posted on November 02, 2015 at 05:44 Hi, I have an STM32F429I-DISCOVERY board and loaded up the example from the STM32Cube package. The example project directory in question isSTM32Cube_FW_F4_V1.9.0\Projects\STM32F429I-Discovery\Ex...

bobert by Associate III
  • 997 Views
  • 1 replies
  • 0 kudos

STM32F030F4 ADC strange behaviour

Posted on October 08, 2015 at 01:01Hello all, I have a custom board with STM32F030F4. I'm trying to run the simplest example generated by STM32Cube, which is to sample Temperature sensor and VRef input using DMA. Everything compiles and runs properl...

srdjan by Associate II
  • 1461 Views
  • 3 replies
  • 0 kudos