User Activity

Posted on November 16, 2015 at 18:54I would like to connect an STM32F405 to usb while running the chip at 1.8V. Since USB requires 3.3V I need some kind of level translator. I have tried the TSX0102 and did not get it working. Has anyone done this b...
Posted on June 01, 2015 at 20:05I've got a 23LC1024 it's a serial ram with spi capabilities http://ww1.microchip.com/downloads/en/DeviceDoc/25142A.pdf I'd like to be able to use it as an extension of my addressable ram on the stm32fxxxx. I have two ...
Posted on February 13, 2015 at 06:54Any idea when tasking vx compiler will be supported in stm cube ?
Posted on October 06, 2014 at 18:57 I have a computer with 64-bit windows 7 installed, when I start the dspin software it has an error message: unable to load spi_sdk.dll The application has failed to start because the side-by-side configuration...
Posted on October 02, 2014 at 22:29I am attempting to run the L6470H discovery kit with the dspin software from a machine with windows xp on it. I was previously able to run it from another machine with xp, I installed the same files but cannot conn...