User Activity

Posted on December 31, 2013 at 11:40HiI'm looking for the libraries to decode and encode mp3 files. But when I use the ST site I'm not able to download the mp3 libraries. It only says active.https://my.st.com//st-extranet-web-active/active/catalog/t...
Posted on December 08, 2014 at 16:06 Hello I'm using a STM32F303CC lqfp 48 on a new product. I'm trying to use 3 Usart channels. I succesfully use channel 1 and 3 but channel 2 is acting weird. In configure the three channels all in the s...
Posted on July 04, 2014 at 13:58The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on June 03, 2014 at 11:30HelloIn our project we need the Spi 3 channel to control an Oled display. The display is connected to pins: D6, B3 and B4 so the Spi 3 pins need to be remapped to those pins.The remapping is done in the spi3 init func...
Posted on May 21, 2014 at 13:48HelloWe have made a custom board which uses a STM32F429II. On that board we also have a SDRAM memory chip of 512Kbit that is connected to the STM32 with the FMC peripheral.We confirmed that the memory chip is working c...