STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLDC faults using Motor Control Library (FOC SDK v4.2)

Posted on October 11, 2016 at 11:31Hello everybody, I am trying to run a BLDC motor with the FOC SDK v4.2, using a STEVAL-IHM021V2 power stage and STMF32F303RE Nucleo board as MCU. I set everything up with no trouble and connect the board to MC Wor...

stm32f4 to stm32f7 port Spi wrong clk signal

Posted on December 12, 2016 at 14:28Hello,until now I have a custom board with a stm32f4 and it works fine with the standard peripheral lib.I tried the new stm32f767 and the board started working after a few changes.Except the SPI, I can receive and...

Hex file code size

Posted on December 13, 2016 at 04:35Hi,I'm using IAR to create a hex file which size is 233KB.However, when I look into the .map file, it told below:183 710 bytes of readonly   code memory    4 265 bytes of  readonly  data memory  62 327 bytes of re...

CubeMX, USB

Posted on November 14, 2016 at 20:52I needed to make a basic bulk device, so the natural starting point appeared to be a CubeMX generated CDC project.   Really, I was stunned by the number of custom files generated:usb_device.h usbd_desc.husbd_cdc_...

stm32f429 register value edit

Posted on December 11, 2016 at 13:44Hi,I want to change the RTC->ISR register value but i could not change it (RTC->ISR = 0xFFFFFFFF etc...). Besides i can change TIM4->CCR1 value. Why rtc register value can not be chaged? Any advise??

er3481 by Senior
  • 898 Views
  • 2 replies
  • 0 kudos

Resolved! reading STM32L15x program counter (with HAL defines?)

Posted on December 12, 2016 at 16:23Question - What is the safest way to 'peek' at the STML152 program counter? Ideally something in the standard HAL files (so no ASM; I am working under AC6 in C). I wish my code to understand if it was loaded/is ru...

STM32F401 - problems with SPI bootloader.

Posted on September 18, 2014 at 18:35Hello!Please, help me! I want to use SPI-bootloader in STM32F401 to update firmware in this controller.But controller returns wrong answers.For my experiments I use demoboard NUCLEO F401RE and application note AN...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.