Skip to main content
valerio2
Associate III
June 13, 2016
Question

STOP reception in UART IO with interrupt

  • June 13, 2016
  • 2 replies
  • 841 views
Posted on June 13, 2016 at 16:56

Hi everybody.

I have an stm32f4 micro trying to communicate with device via UART. I want to receive with interrupts and possibly, based on some conditions, stop the reception process (i.e. if some time expires from the last \n received). Since I am reading one char at once (receiving variable length strings) and the reception is called again within the callback (see https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fBest%20way%20to%20use%20HAL%20UART%20Receiver%20IT%20Function&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=18255), I have to stop it outside the callback. Unfortunately I am not able to do that, this causing an overrun error next time I start reception again (since the conditions allow to do that), and I am a little stuck. I tried with something like

__HAL_UART_DISABLE_IT(&UART_MOBILE_Handle, UART_IT_RXNE);
__HAL_UART_DISABLE_IT(&UART_MOBILE_Handle, UART_IT_PE);
__HAL_UART_DISABLE_IT(&UART_MOBILE_Handle, UART_IT_ERR);

but it seems not working. Does anybody have any suggestion? Thank you and regards.
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    June 13, 2016
    Posted on June 13, 2016 at 17:22

    Turning off the RXNE isn't going to stop the sending device sending data, nor the USART from trying to receive it. For that consider flow-control, ie CTS/RTS or DTR/DSR type implementations.

    The USART RE (Receive Enable) is part of control register, this would stop the USART from attempting to receive data, but might result in framing or loss of data issues if the sending side isn't cooperating.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    valerio2
    valerio2Author
    Associate III
    June 14, 2016
    Posted on June 14, 2016 at 08:39

    Thank you Clive for your advise. Actually I can't use a flow control mechanism because of the board I am working on: no RTS/CTS or DTR/DSR lines have been used to connect the module with the micro, and clearly I can't change it :).

    However to be more precise I have implemented a mechanism like

    
    .
    
    .
    
    .
    
    SIM3560E_IO_Read_IT(&mobileRxSingle, 1);
    
    
    currentTick = osKernelSysTick();
    
    
    while
    (osKernelSysTick() - currentTick < LFTIMEOUT)
    
    {
    
    if
    (mobileRxReady != SET)
    
    currentTick = osKernelSysTick();
    
    }
    
    
    mobileRxReady = RESET;
    
    
    StopReceive_IT();
    
    .
    
    .
    
    .

    where

    osKernelSysTick()

    belongs to the RTOS HAL middleware and is similar to HAL_GetTick(). The reception callback is

    
    void
    mobileReceiveCallback(UART_HandleTypeDef *huart)
    
    {
    
    ringBufferPushSingle(&mobileRxBuffer, mobileRxSingle);
    
    
    SIM3560E_IO_Read_IT(&mobileRxSingle, 1);
    
    
    if
    (mobileRxSingle == 
    '
    '
    )
    
    mobileRxReady = SET;
    
    }

    Everytime a is received

    currentTick

    is reset and the while loop keeps going on. If a is received

    currentTick

    is not reset and if the module doesn't throw any other char within

    LFTIMEOUT,

    then the while loop is exited and I need to stop reception (clearly I need a global timeout to avoid waiting forever if the module is not replying anything). I have not came up with any other mechanism to do that with interrupts (the problem is that reception is retriggered everytime the callback is reentered): this modulethrows strings terminating with BUT several might be put within a string, so the only way it seems to me I can do to identify an end string is with a timeout. Maybe a reception with polling would be a better way but I wanted to investigate the implementation with interrupts.