STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with Mounting and IDEs for STM32F429ZIT6

Posted on December 09, 2016 at 12:57Hi all,I am new to microcontroller programming, and i recently started working on STM32F429ZIT6 MCU.I could able to program the Discovery board with sample programs(Blinking LEDs) with Kiel IDE, though i am facing...

implementing swd with spi on stm32f3

Posted on November 29, 2016 at 03:44I have a working bit-banged implementation of swd, now I want to use the spi device.  The protocol is a bit odd in requiring some short input sequences.  Essentially, I'm using the spi device for everything that's...

STM32F070 USB CDC Example

Posted on October 07, 2016 at 13:13Hello, I am using STM32F070 microcontroller and current implementing USB CDC, I was searching a basic example of USB CDC on STM32F0, but not able to find any appropriate one, any help in this regard would be highl...

USB circuit

Posted on December 10, 2016 at 13:32Hello, I'm trying to use the usb peripheral embedded in stm32f407vgt6 as device. I connected D+(from host) to D+(of my MC) through 22Ohm resistor and D-(from host) to D-(of my MC) through 22Ohm resistor also Vbus(...

DFSDM conversion resolution problem

Posted on December 08, 2016 at 22:32Hi,I am trying to build something and currently doing some evaluation and development with 32L476GDISCOVERY Discovery Kit with STM32L476VG microcontroller.What I am trying to achieve at the moment is output of int...

stm32f3/4 maximum gpio read write operation

Posted on November 09, 2016 at 18:55HelloAs i inspected through assembly instructions, it is possible to read 16 bits gpio port with 2 cpu cycles and write with 4 cpu cycles, beside of electrical considerations, is it possible to achieve reading and...

DMA on SPI

Posted on November 11, 2016 at 14:20Hello,I have one question. I have two CPUs (STM32F407 + STM32F103) and I need to ''share'' (or better say ''synchronize'') 64 bytes between these CPUs every 100us. So every 100us the CPU must send 64 bytes to anot...

Bad SPI clock duration in stm32f746

Posted on November 11, 2016 at 18:08Hello. I have got stm32f746 and I make project with cubeMX. I  want to use SPI4, SPI5, SPI6 as fullduplex master with 50Mb/s baudrate. Then I try to HAL_SPI_Transmit(&hspi4, pData, 1, 30000); in while(1) cycle. ...

ldpr by Associate
  • 1612 Views
  • 2 replies
  • 0 kudos

STM32F3 - Sending Sine Wave with DAC and DMA

Posted on November 29, 2016 at 05:51 Hello! I am currently trying to send a sine wave through the DAC. I've tried both using the std peripheral libraries and stm32cube, but to no avail. The frequencies and amplitude of the measured sine w...

kl4971tse by Associate II
  • 3541 Views
  • 4 replies
  • 0 kudos

How do I switch PLLSource once it is running?

Posted on December 07, 2016 at 22:19Hi, I want to start off my STM32F745VET6 running on the PLL sourced from the 16MHZ HSI oscillator. I need to run some I2C code to initialize an external multi-output high accuracy clock generator chip where one of...