STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 with an ADAFRUIT BLE SPI

Hello st community,I'm trying to set up a bleutooth communication between my phone and my stm32 with the Adafruit module in SPI communication, but I'm having a problem.When I use my arduino and the demo code it works perfectly but when I connect to m...

Capture d'écran 2024-12-11 120927.png
Paulo971 by Associate III
  • 14225 Views
  • 21 replies
  • 2 kudos

Resolved! STM32G070KB PA8 and PA9 interaction

Hello,We have run into a weird behaviour with the STM32G070KB. With PA8 defined as an input with internal pullup and PA9 as output push-pull. When PA9 is at low level and PA8 unconnected, PA8 is at VCC (3.3V) as expected.When PA9 is at high level, PA...

Trilys by Associate II
  • 6911 Views
  • 11 replies
  • 0 kudos

Resolved! Replacement for STM32F105

We're looking to replace our F105 processors in the next generation of a an automotive application.We want more flash,2 I2c ports2 SPI ports3 UARTspreferably 4 CAN ports, but atleast 3, 2 of the CAN ports should support CAN-FDand more hardware securi...

DanielNslund_0-1738222225864.png