STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EmbSysRegister plugin for STM32F7

Posted on March 01, 2017 at 08:06Hi,does anybody have the STM32F7's xml file for the EmbSysRegister Plugin of Eclipse or know where i can find it?Thanks

sascha23 by Associate II
  • 510 Views
  • 0 replies
  • 0 kudos

Memory protection around location 0

Posted on February 28, 2017 at 19:57I've been putting together an article on DMA and one of my examples uses DMA to CRC the Flash memory array of a '407 processor.In comparing the speed of DMA to iterative assignment, I found that DMA will succeed i...

STM32 CanBus cannot get out of interrupt handler

Posted on February 28, 2017 at 12:01hello dear forum,  I try to make CANBUS of http://www.mikrocontroller.net/part/STM32F103RC work I managed to make CANBUS send message in loopback mode however when I turn on receive interrupt the processor hangs a...

HAL I2C example from I2C_TwoBoards_ComIT

Posted on February 28, 2017 at 18:59I am having trouble following the example code as given for the CubeMXHow does it not get stuck in the while(1) loop in the main function? I understand that it is an interrupt, but the only thing that the function...

achin by Associate II
  • 1266 Views
  • 1 replies
  • 0 kudos

CubeMx problems with USER CODE SECTIONs

Posted on February 26, 2017 at 04:16HII am using Cube32MX for the implementation of a USB Host + Fatfs to work with a pendrive connected to a stm32f407, generate code for SW4STM32 but in the usb_host.c file generated by Cube32MX the following appear...