Posted on August 31, 2016 at 14:17
I'm having a problem getting an accurate reading from the ADC with a reduced PCLK. The readings are about 800 values higher than what is expected (using 12bit ADC). When the microcontroller is running at 48MHz ...
Posted on September 01, 2016 at 15:55After looking into it more, I found the cause of the problem. I'm currently using PA1 as an output. When this pin is configured as an output, the reading of the ADC jumps up, until it's configured as an input a...