2016-09-02 12:10 AM
Hello,
I am using gsm module to transmit a message using USART of stm32f303. I have used following commands for gsmAT+CMGF=1AT+CMGS=''+923046761738''at the end it requires CTRL+Z to send the message but usart is not sending the ctrl+z i am attacting my code please help me''char configuration[150];char configuration[]=''AT+CMGF=1\r\n\0'';char message[150];void RCC_Configuration(void){ /* Enable GPIO clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /* Enable USART clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);} /**************************************************************************************/ void GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure; /* Connect PA9 to USART1_Tx */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_7); /* Connect PA10 to USART1_Rx */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_7); /* Configure USART Tx as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure USART Rx as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_Init(GPIOA, &GPIO_InitStructure);} /**************************************************************************************/ void USART1_Configuration(void){ USART_InitTypeDef USART_InitStructure; /* USART resources configuration (Clock, GPIO pins and USART registers) ----*/ /* USART configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - One Stop Bit - No parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; /* USART configuration */ USART_Init(USART1, &USART_InitStructure); /* Enable USART */ USART_Cmd(USART1, ENABLE);}void gsm_message(char *ptr){ while(*ptr) { while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty USART_SendData(USART1, *ptr); ptr++; } }int main(void){ // RCC_Configuration(); GPIO_Configuration(); USART1_Configuration(); //while(1) //{ gsm_message(''AT+CMGF=1\r\n''); //Delay(1); gsm_message(''AT+CMGS=\''+923046761738\''\r\n''); //Delay(10); gsm_message(''hello''); while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty USART_SendData(USART1,(char)0x1A); gsm_message(''\r\n''); //Delay(10); //} while(1); // Don't want to exit} #i2c #stm32f303vct6 #stm32f3We’re moving the ST Community to a new platform to give you a better and more reliable community experience.