STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FATFs f_open ?

Posted on February 25, 2017 at 23:02Everybody,Why isn't my f_open working properly ?I tried the example from UM1718 but stack on f_open.Is SDIO initialized properly ?here's the code :/TEST SDIO beginif(retSD == 0)            {                printf(...

Coupling between GPIO lines

Posted on March 01, 2017 at 15:28Hi,I have a strange issue with GPIO on Nucleo-64 stm32F401RE.I implement SPI protocol on it and each line of the GPIO is perform very well.While I connect a bride to those pins the data line make the EN line noisy. I...

nirb by Associate II
  • 1989 Views
  • 4 replies
  • 0 kudos

Resolved! two USART configuration failed (USART3 problem)

Posted on March 01, 2017 at 15:27Hi,Here is my code for configuring two different usart but my USART3 doesn't work properly and USART2 works fine.(I remap both of them). what is my mistake that I didn't pay attention?Problem: I don't have any signal...

parisa by Senior
  • 1963 Views
  • 6 replies
  • 0 kudos

Problem measuring two signals frequencies

Posted on February 28, 2017 at 08:47Hello everyone,I would like to measure frequency of two different signals using STM32Fxx timers'but i have problems setting two different timers to work simultaneously .thanks for your help.

STM32F103C8T6 SPI communication with ADS1220 stops

Posted on March 01, 2017 at 01:17Hello,I'am using and STM32F103C8T6 development board to communicate via SPI with ADS1220(Analog to Digital Converter). My code needs to read the buffer of the ADS1220 at certain times. When i run the code the SPI wor...

bla vbla by Associate
  • 5902 Views
  • 3 replies
  • 0 kudos

What is the name of this forum?

Posted on March 01, 2017 at 12:55It is not very clear what is the forum currently in use. It is a common problem, many discussions are started in both forums. Or is there 3 forums.I use Firefox browser with ads blocker and the name of the current fo...

LMI2 by Lead
  • 1049 Views
  • 1 replies
  • 0 kudos

RTC in STM32L152RET6

Posted on February 28, 2017 at 07:52hi WE ARE USING STM32L152RET6.Is it have internal RTC?Why  RTC_REFINRTC_TA RTC_OUT    pins are used?Kindly provide any rtc document for STM32L152RET6

STM32F7 casual PWM period

Posted on March 01, 2017 at 11:02Hello, I'm a new member on the forum.I'm working on a stm32f7 and I need to generate a 10 kHz PWM from TIMER 13. I have a very strange problem. Sometimes when I turn on my board, the PWM period is totally wrong, it i...

Backup SRAM content lost in VBAT-mode

Posted on February 28, 2017 at 12:09Are VCAP_1 and VCAP_2 used in Vbat-mode?I have an issue with the content of the Backup SRAM is lost when i power down the device, even though the Vbat is active.If i do a reset the content of backup SRAM and RTC-r...

mats by Associate
  • 1988 Views
  • 3 replies
  • 0 kudos

HAL_SPI_TransmitReceive

Posted on June 03, 2016 at 01:54I'm having some peculiar behavior using the polling mode spin routines (F3), so I took a look at the HAL code.      I'm sending 8 bit data using an array of 8-bit quantities.  Inside the TransmitReceive routine I see ...