STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA - Pheriperal to Memory max Speed

Posted on March 27, 2017 at 14:16Hi,I'm using a STM32F429 operating at 168 MHz. I want to read in 16 GPIO pins (one port) via DMA. I'm curious what's the maximum input rate is, for a certain number of consecutive level changes (read out of an extern...

Skadi F by Associate II
  • 2530 Views
  • 4 replies
  • 0 kudos

stm32f301 comparator

Posted on March 28, 2017 at 12:59I'm trying to use stm32f301 comparator 2, but the output is always 0 no matter if the two inputs are higher or lower. I guess the configuration is wrong.The main code is here. Thanks for the help in advance!void Conf...

NT7502 driver (LCD driver)

Posted on March 28, 2017 at 13:15mostafa.fathihii want to drive an LCD. my LCD driver is NT7502. i want to know what can i drive it with stm32f103 AND STemwin? if no then how do i do?thankfulnull

SPI Packing Mode

Posted on March 26, 2017 at 17:43Hi all,i am using the STM32F030RC for a customer project. To SPI1 we have connected a SPI-Flash device (SST25VF040B). I am using Cube MX (4.19) to generate as much initialization code as possible.So i have configured...

tj by Associate II
  • 1741 Views
  • 2 replies
  • 0 kudos

STM32F103 CPU loses external IO interrupt.

Posted on March 28, 2017 at 08:26Hi.I am using the STM32F103VBT6 CPU and STM32F10x_StdPeriph_Driver.I want to receive one external IO interrupt and operate 4 PWM channels at the same time.I set the EXTI port as below and created the interrupt ISR fu...

Configure System Clock STM32F0XX

Posted on March 27, 2017 at 19:30Dear All. I'm using STM32F051 with 12 MHz crystal. but my serial communication ran 1.5X faster then i set.I think i need to configure HSE. i have editted ->  #define HSE_VALUE    ((uint32_t)12000000) but still doesn'...

STM32F407VGT6 China Board not working - Tips?

Posted on March 25, 2017 at 19:16I have a Discovery F4 Board and purchased recently a China Board from *bay (Ebay-Artikel Nr. 272501820584?) with the same uC (STM32F407VGT6). I thought a cheap way to test my code and put it into my project. I have a...

problem with NVIC_SystemReset

Posted on March 24, 2017 at 14:47Hi everybody,I'm using a STM32F205VE on one of my electronic board.I'd like to reset my microcontroller, so I use the function NVIC_SystemReset that I can find in core_cm3.h but it never works.My board is not resetti...

STM32L051/STM32L053 adc multichannel

Posted on December 15, 2014 at 14:24hi everyone, are there any examples how to read individual adc values on more than one channel for the stm32l051/stm32l053 microcontroller. i'm using the stm32l0538 discovery board and i also checked the examples ...

HAL bug

Posted on March 27, 2017 at 16:50is there any formal way to report bugs?

John Doe1 by Associate III
  • 1118 Views
  • 1 replies
  • 1 kudos