cancel
Showing results for 
Search instead for 
Did you mean: 

USB: when would you need more than one interface?

Vu.Andy
Associate III
Posted on September 19, 2016 at 22:52

I've seen a lot of examples and almost all of them from STM have only a single interface.

And it seems like most of the time, one interface should be enough.

Since I am still learning USB, for those who have experiences with USB, when would there be a need for more than one interface?

For example, if I am building a HID Audio device, does it need more than one interface? 

Thanks.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
tsuneo
Senior
Posted on September 20, 2016 at 03:08

When a device require two or more USB functions, it is equipped as a composite device.

A couple of popular examples, maybe on your desktop,

A) USB Audio + HID consumer device

- Audio amplifier/speaker with a volume knob and a mute switch.

The status of the volume knob and the mute switch is passed to PC over a HID consumer device.

B) HID keyboard + HID consumer/system devices

- PC keyboard with audio control / sleep-wakeup keys

Windows force keyboard in a single interface. And then, other keys, supported by HID consumer/system devices, should move into another separated interface.

C) UVC (USB Video class) + audio

- Web camera with microphones

D) Vendor (debug) class + MSC (Mass-Storage class) + CDC

- ST-Link/V2-1 with mbed support on Nucleo and recent Discovery boards

E) Your USB device with DFU (Device Firmware Upgrade)

etc.

Tsuneo