STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401 on custom board. USB doesn't work

Posted on March 24, 2017 at 19:16Hi everybody,This is my first question, I really hope you can help.I soldered a STM32F401RC on my custom board and I connected it to a mini-usb plug. In particular, I connected PA9 to Vbus, PA11 (configured as USB_OT...

STM32F4 + FreeRTOS + usage fault

Posted on March 29, 2017 at 12:41FreeRTOS + STM32F4I have been hitting a usage fault with CFSR invpc bit set which according to documentation means that an error occurred returning from an exception and that the stacked pc indicates the faulting ins...

Need .dfu from IAR when mapped to the ITCM interface

Posted on March 29, 2017 at 10:32What must I do from IAR to make a file which will properly convert to a .dfu file which will burn onto my board using the DFUSE demo - realizing that we are mapped to the ICTM interface?We are using the STM32 32-bit ...

Is it possible to create an Exact 1ms wakeup period using RTC in Stm32l1 series controller? if yes, How it can be done? 

Posted on March 24, 2017 at 12:35(ref: AN4759)Configuration 1 - able to achieve ~1ms but not exactly 1 ms.Configuration 2 - not able to achieve 1 ms but successfully achieved 1s as the least period and can program in multiples of it.

STM32F105 - Create USB Virtual COM port

Posted on March 14, 2015 at 22:11Hi,I am using a Decawave EVK1000 and would like to create a USB VCOM port to my PC.I have never made a USB driver before and have downloaded the USB FS library for the STM32F105.From the library I see there is the De...

mati by Associate
  • 1533 Views
  • 1 replies
  • 0 kudos

TIMx TRGO generation

Posted on March 28, 2017 at 23:39On my '407 I am using TIM2 to trigger a series of ADC conversions. The connection between TIM2 and the ADCs is TRGO.I have set up the time base for TIM2 to be 84MHz and TIM2 has no prescaler and a counter period of 2...

Resolved! STM32 chip revision

Posted on March 24, 2017 at 16:35I have a NUCELO board with STM32F767ZI.I have read that there are http://www.st.com/content/ccc/resource/technical/document/errata_sheet/group0/23/a6/11/0b/30/24/46/a5/DM00257543/files/DM00257543.pdf/jcr:content/tran...

SPWF01SA.21 WiFi module

Posted on March 28, 2017 at 16:31Is it possible to connect an external eeprom to the SPWF01.21 module? The stored eeprom data will be very small >1K and only serve to remember GPIO high or low settings of the modules STM32F103 core that an end user ...

Resolved! STM32F334 and RTC Setup

Posted on March 28, 2017 at 10:35Hi,I have a STM32F334 with a cylindrical watch 32.768kHz xtal connected as a LSE oscillator. LSE now works. Folks on the forum, were kind enough to point out to me about possible PCB related issues.Originally, I've h...