User Activity

Posted on September 17, 2016 at 14:55Hello,I would like to develop with the STM32L476RG and I have tried a few IDE without success. Everything is up to date.Building the project fails with KEIL : *** Using Compiler 'V5.06 update 3 (build 300)', fold...
Posted on July 09, 2016 at 09:31CubeMX V4.15.1I would like to create a new project using an old firmware package for my STM32F4 (1.11.0 or older for instance). I can't find a way to select the version of the package in the project settings.Regards,P...
Posted on December 30, 2014 at 12:07Hello,I am programming a shell based on HAL UART and I experienced difficulties with the HAL UART API provided with CUBEMX. I was using the non-blocking UART Reveice IO function (IT mode).I have modified the CUBEM...