STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CubeMX 4.20.0 Problem

Posted on March 14, 2017 at 08:18I think the new issue seems to have a problem with source generation.When choosing the HSE, create the source as follows :  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;To operate ...

Resolved! HSE Bypass Clock Source w/CubeMX and Nucleo 303ZE fails

Posted on March 27, 2017 at 01:42Possible bug in CubeMX 4.20.0?Using Nucleo 303ZE board, and Atollic 7.1.1Build dead simple default project, except in RCC, set High Speed Clock to 'BYPASS Clock Source', and select HSE as input to PLL.In main.c you'l...

Changing clock source from HSE to HSI

Posted on August 26, 2015 at 08:16Hi Please refer below code to change clock source from external HSE to internal HSI /* Enable HSE Oscillator and activate PLL with HSE as source */#if 0 // Choose External Crystal (HSE) As Source RCC_OscInitStruct.O...

sangamesh by Associate II
  • 3218 Views
  • 5 replies
  • 0 kudos

HAL Timer PWM DMA Completion

Posted on April 27, 2017 at 23:34 I have an app running on F303 where i build an waveform buffer of PWM widths (CCR1) and then periodically send the waveform using HAL_TIM_PWM_Start_DMA. Project is CUBE generated.It all works find, resending the ...

32L476GDISCOVERY doesn't boot?

Posted on April 27, 2017 at 13:52I received my 32L476GDISCOVERY and followed step 1 on the answer card to power the board using the USB mini-B connector. LD1 starts flashing slowly but nothing else happens. Nothing displays on the LCD screen as the ...

Suitable low power BLDC motor for Nucleo-IHM11M1

Posted on April 27, 2017 at 13:07I'm looking for a low power BLDC motor for use with a X-Nucleo-IHM11M1 motor control board. Specification says 10 V max and 1.3 A max about 13 W give or take. The documents say the STSPIN230 chip could be used in bat...