STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is DMA Double Buffer Mode only Peripheral to Memory?

Posted on July 28, 2017 at 14:40It appears from the (rather lacking) documentation that the DMA Double Buffer Mode is only a Peripheral to Memory transaction. Is this correct? Or can I use double buffering from memory to peripheral?

STM32F4x FMC guidelines

Posted on July 31, 2017 at 04:42Hello,I currently designing a board using STM32F469BETx and two SDRAM ICs. I would like to know if ST provides any guidelines or application notes for FMC wiring and connections to the memories?Thank you.#fmc #stm32f4...

Resolved! STemWin scrambled display

Posted on July 28, 2017 at 14:50I am trying to use STemWin 532 on a STM32f467 board. I created a framewin with 4 buttons using GuiBuilder and ran the application, but the display is scrambled. This is how a framewin with 4 buttons looks like on my d...

STM32F4 to FPGA via FSMC

Posted on April 27, 2016 at 15:43Hi all,I'm just starting to embark on the problem of accessing external registers (implemented in a FPGA), via the FSMC on the STM32F4 core.  What I'm interested in doing is accessing these registers as SRAM (memory ...

psdeering by Associate II
  • 11311 Views
  • 9 replies
  • 0 kudos

Too slow for Input Capture? 1Hz

Posted on July 19, 2017 at 14:17Looking to measure duty cycle of a pin where I'm looking for a pulse anywhere between 200miliseconds and 800 miliseconds on a 1Hz period. I think I used the terminology correctly, sorry if I didn't. Much of the time, ...

Resolved! ADC1 vs. ADC3 behavior

Posted on July 26, 2017 at 09:50Hi,I'm using STM32F427ZI with FreeRTOS.I am configuring both ADC1 and ADC3 to run using DMA, but I'm getting different behavior between them. This is the configuration for ADC3, ADC1 is configuration the same:ADC1 is ...

0690X00000607gDQAQ.png 0690X00000607gIQAQ.png
Maor Avni by Associate II
  • 3700 Views
  • 6 replies
  • 0 kudos