STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Too slow for Input Capture? 1Hz

Posted on July 19, 2017 at 14:17Looking to measure duty cycle of a pin where I'm looking for a pulse anywhere between 200miliseconds and 800 miliseconds on a 1Hz period. I think I used the terminology correctly, sorry if I didn't. Much of the time, ...

Resolved! ADC1 vs. ADC3 behavior

Posted on July 26, 2017 at 09:50Hi,I'm using STM32F427ZI with FreeRTOS.I am configuring both ADC1 and ADC3 to run using DMA, but I'm getting different behavior between them. This is the configuration for ADC3, ADC1 is configuration the same:ADC1 is ...

0690X00000607gDQAQ.png 0690X00000607gIQAQ.png
Maor Avni by Associate II
  • 3730 Views
  • 6 replies
  • 0 kudos

Resolved! Problem with PD9 by FSMC Interface on Nucleo-F413ZH board

Posted on July 28, 2017 at 20:16HelloI'm using a Nucleo-F413ZH board with System Workbench for STM32, Currently I try to startup the FSMC Interfcae 16 Bit for my QVGA Display with SSD2119. I config the Ports and the FSMC peripheral OK DB15 (PD10 is ...

Resolved! SDIO INTERFACES IN STM32F407VG

Posted on July 25, 2017 at 13:16HOW MANY SDIO INTERFACES ARE THEIR IN STM32F407VG ????ONLY ONE OR TWO??IF TWO ARE THEIR CAN I USE BOTH AT SAME TIME??       https://community.st.com/community/stm32-community/stm32-forum?sr=search&searchId=521dc8c2-71...

STM32 + �?¡�?�N

Posted on July 28, 2017 at 22:25  The original post was too long to process during our migration. Please click on the attachment to read the original post.

Resolved! I2S CLK Outputs on nucleo-F446RE

Posted on July 13, 2017 at 18:21The original post was too long to process during our migration. Please click on the attachment to read the original post.

ad ho by Associate III
  • 3991 Views
  • 7 replies
  • 0 kudos

Wav player using DAC in STM32F429

Posted on July 26, 2017 at 13:32Hello,I noticed that the stm32F429 disco does not have the CS43L22 circuit nor a 3.5mm jack for audio output as its rival the F407, but it has two internal DAC output, which can be used to play a wav file.If anyone ha...

Using Vbat as ADC for battery level monitoring

Posted on July 27, 2017 at 05:18I'm updating an old PCB design that used the STM32L432KB. The new design is using the STM32L452CE which has the Vbat pin.In the old design I used a voltage divider across the battery and connected it to an ADC pin to ...