STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 70F6 won't start after reset

Posted on August 12, 2017 at 03:38so i got a 70F6 uC wired up to an LED and a simple program to make it flash. i plug it into power and the program executes, but then when i hit the reset button to connect the NRST pin to ground the flashing stops a...

SW4STM32 imported project name problem

Posted on August 11, 2017 at 19:40I have a SW4STM32 problem that all project names of imported example from STM32Cube_FW_F0_V1.8.0 become same board name, such as STM32F072RB-Nucleo.I can import ONE example in ONE workspace but I would like to impor...

quadrature encoder

Posted on August 10, 2017 at 19:48hi everyone i have configured the timer for quadrature encoder which is working but as my quadrature encoder resolution is 1920 counts in 360 degree but in debugging mode it is give me 180 counts per 360 degree my c...

waaizkhan by Associate III
  • 1829 Views
  • 3 replies
  • 0 kudos

SAI Rx DMA w/ CIRC does not Recirculate

Posted on August 11, 2017 at 21:01I am using the SAI1 peripheral on the STM32469I for full-duplex operation.  I first implemented independent Tx, and it works great.  However, when I add synchronous slave receive, the DMA acts very strangely.  Inste...

HAL_I2C_Mem_ReadDMA stuck reading large amount of data

Posted on August 11, 2017 at 13:20Hi, new to the forum.STM32L476: when reading a block larger than 255 bytes from an EEPROM , HAL gets stuck in HAL_I2C_STATE_BUSY_RX, SCL low, SDA high. Reload was setup alright in HAL and in STM32 I2C the TCR flag i...

straubm by Associate III
  • 1287 Views
  • 2 replies
  • 0 kudos

STM32F103 ADC INTERRUPT from timer 1 CC1 doesn't start with HAL_ADC_START_IT().Adding HAL_ADC_START() after HAL_ADC_START_IT() Solves the problem. Why?

Posted on August 11, 2017 at 14:55I don't see the EOC interrupt stepping into action when using only START_IT().Using MXCube, attached is my user code.Haven't modified any header files. only the weak callback functions which are in my code.

Chen BH by Associate
  • 941 Views
  • 1 replies
  • 0 kudos

SD Card failing 'disk_initialize' in standalone mode

Posted on August 11, 2017 at 03:25I have an ST STM32F405 microprocessor. I generated my IAR Embedded Workbench 7.4 files using STM32 Cube software.  I'm trying to use the SD card resources to access a micro SD card on our custom board. When I use th...

Eric P by Associate
  • 1033 Views
  • 1 replies
  • 0 kudos

stm 32f 103 cubmx dma

Posted on August 11, 2017 at 14:36i need help for start used cubmx enable dma for read from spi 1 and write on spi 2if any one can help to me for fined reference document and examplethanks

STM32L1 internal temperature

Posted on August 09, 2017 at 14:44Hello,I use a STM32L151RCT6 on a custom board and i want to read the internal temperature. In the cube library I found an exemple using the LL library so I included the ll_adc driver in my code and tried to use it.W...