STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32746G RTC problem

Posted on August 10, 2017 at 08:56Hi Everyone,I am working on RTC with stm32f746g controller. I tried number of option but i am not getting accurate time.After some time rtc is getting lag of 4 to 5 seconds and it keep on lagging in time.I am using ...

Virtual Serial port for STLink V2

Posted on August 12, 2017 at 15:46As I mentioned in the subject, I would like to know whether STLink V2's firmware can be updated to support Virtual COM port as like the STLink V2-1 (STLink V2-A) supports. I have two STM32F development boards namely...

Resolved! How to use VREFINT with CubeMX

Posted on August 10, 2017 at 07:44Thank you for your patronage. I want 1.2 V in operational amplifier circuit. so, I want to use VREFINT as 1.2V.But I don't know how to use VREFINT.  I don't know how to output VREFINT with Cube MX. I am using STM32F...

0690X00000607nEQAQ.png 0690X00000607nOQAQ.png
Ken Inoue by Associate III
  • 1873 Views
  • 3 replies
  • 0 kudos

Disable PHY initialization and configuration

Posted on August 12, 2017 at 07:15I'm using CubeMX version 4.22 and firmware FW_F4 V1.16.0. I'm using a STM32F427 and a MICREL KSZ8863MLL Integrated 3-Port 10/100 Managed Switch with PHYs. Everything is working fine. The problem I have is with the t...

Resolved! 70F6 won't start after reset

Posted on August 12, 2017 at 03:38so i got a 70F6 uC wired up to an LED and a simple program to make it flash. i plug it into power and the program executes, but then when i hit the reset button to connect the NRST pin to ground the flashing stops a...

SW4STM32 imported project name problem

Posted on August 11, 2017 at 19:40I have a SW4STM32 problem that all project names of imported example from STM32Cube_FW_F0_V1.8.0 become same board name, such as STM32F072RB-Nucleo.I can import ONE example in ONE workspace but I would like to impor...

quadrature encoder

Posted on August 10, 2017 at 19:48hi everyone i have configured the timer for quadrature encoder which is working but as my quadrature encoder resolution is 1920 counts in 360 degree but in debugging mode it is give me 180 counts per 360 degree my c...

waaizkhan by Associate III
  • 1804 Views
  • 3 replies
  • 0 kudos

SAI Rx DMA w/ CIRC does not Recirculate

Posted on August 11, 2017 at 21:01I am using the SAI1 peripheral on the STM32469I for full-duplex operation.  I first implemented independent Tx, and it works great.  However, when I add synchronous slave receive, the DMA acts very strangely.  Inste...