User Activity

Posted on August 28, 2017 at 09:53Hi,     I m using FT6236 capacitive touch screen controller with I2C3 inside STM32F407. All required Connections have been checked thoroughly. I have referred the reference code from all possible links available fro...
Posted on August 01, 2017 at 10:31Dear all,              i need to monitor ADC & display the value continuously in Text box using STEmwin Generated code. My ADC driver, handling for low threshold & high threshold value is working correctly as per te...
Posted on July 25, 2017 at 11:21Dear all,              i want to generate .hex or .bin file using Keil-MDK ARM  for external NOR flash connected with STM32F746NG in STM32F746G-Discovery Kit. I know how to program both after getting generated but i d...
Posted on July 20, 2017 at 12:55Refering to page no 167 in en.DM00124865.pdf  which is available as STM32F746NG USER MANUAL. These are following typo errors are found as follows:Bit 10 ADC3EN: ADC3 clock enableThis bit is set and cleared by software...
Posted on July 19, 2017 at 14:11Refering to page no 6 in  mb1191.pdf  which is available as STM32F746G-discovery Kit schematic. The pin diagram of following two Arduino connector was incorrect, this need correction as follows:1. CN4 connector has AR...