STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Flash layout of an STM32F469IEH with 512kB Flash?

Posted on June 19, 2017 at 12:01Hi,we want to use the STM32F469IEH controller which has 512kB of Flash Memory. The Reference Manual does not show any Flash Layout of the 512kB Flash. I assume that it has the Layout of the 1MB Flash Memory with 1x512...

andi z by Associate II
  • 2086 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CUBEMX

Posted on August 10, 2017 at 15:35Hi,Does the STM32CUBEMX support STM32L072KZ or any other MCU from STM32L0x2  series that has 128k of flash?I didnt find those MCU's...thanks...

kobi nis by Associate
  • 1451 Views
  • 2 replies
  • 0 kudos

USB dual host application's problems by STM32F205

Posted on August 07, 2017 at 02:46Can I use dual USB host by ST's MCU(STM32F205RE)? Will it supported two USB interface to make two FS host controller (one is FS, another is HS and didn't use external phy)? have one have any suggestions about this? ...

david wu by Associate
  • 1070 Views
  • 1 replies
  • 0 kudos

[CubeMX Request] Move init functions from main.c

Posted on August 10, 2017 at 09:36As title says, this a request to move generated functions SystemClock_Config and LL_Init (when LL is used) from main.c to peripheral file, if 'Generate peripheral initialization as a pair of '.c/.h' files per periph...

George.P by Associate III
  • 1942 Views
  • 3 replies
  • 0 kudos

I2c cannot read from sensor

Posted on August 03, 2017 at 06:49 I am using mlx90614 sensor attached to my nucleo F091RC. I have a working code with mbed : double mlx90614::read_temp(uint8_t reg) { char cmd[2]; cmd[0] = 0x01; cmd[1] = 0x00; // Send start bit __i...

STM32F0 Discovery Flash Download Error!

Posted on August 10, 2017 at 10:39Hello to everyone. I am using Stm32f0 discovery (ST-Link) for the programmer. I will load the to external processor (STM32L011D3P6). I edited the Flash settings in Keil IDE. I get this error:'' Debugger - Cortex M E...

0690X00000607l9QAA.png

STM32F0 SPI transmit via interrupt

Posted on August 09, 2017 at 11:30Hello everyone,I'm useing the NUCLEO-F072RB and I'm trying to get the SPI via interrupts to work.Here is the CubeMX initialization of the SPI:/* SPI1 init function */void MX_SPI1_Init(void){      hspi1.Instance = SP...

PaKi by Associate II
  • 1435 Views
  • 2 replies
  • 0 kudos