2017-04-14 4:50 AM
Hi,
I am testing CAN interface on STM32F769i-Eval board.
I have created a CAN Application and i can able to receive CANpackets on the PC Application in Loopback mode.
Unable to receive messages in Normal mode.
Moreover in Loopback mode, I am unable to receive CANpackets from PC to board.
Am using kvaser tool and application for seeing messages on PC
Is there any additional configuration is required in evk to get the CAN packets in CN26 connector?
Thanks and Regards
Rizwan Syed
2017-04-14 5:40 AM
Hello,
Please refrain from posting the same question again.
If you have precision to ask, do so on the same thread...