STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MDMA Transfer

Hello and good year everyone,I am trying to follow the architecture below, where I read 1 ADC halfword at 2KHz via SPI. The idea is to trigger the DMA 1 Channel 3 as soon a new data is available in my SPI. It transfers my data from SPI to RAM. As soo...

MonsieurShann_0-1736343982098.png

Pointers on Designing TFT Based System for STM32H750XB

Hello All,               I need to design a board that will carry an IS42S32400F-6BL SRAM ,STM32H750XB MCU,Flash MT25QL512ABB1EW9-0SIT and Couple of support components along with Power supply.My questions-1) MCU Power Supply Protection2) High frequen...

Caan by Senior
  • 837 Views
  • 3 replies
  • 0 kudos

Resolved! STM32U0 timer clocks x2

In contrast to the STM32L0 that I am migrating from to the newer STM32U083, the U0 clock tree (Reference manual RM0503 V2.0 figure 11) does NOT show that timer clocks are PCLK*2 when APB prescaler>1.Also, it states in 5.2.14 that timer clock TIMPCLK ...

Hans_W by Associate III
  • 5801 Views
  • 16 replies
  • 2 kudos

ADCs - QUEUE

Hello,  I have a NUCLEO U545 - REQ and i have a Queue in which i read the incoming values from 4 potientiometers from my ADC4 and send them directly into the DMA.  The problem is that i also have the ADC1 connected to some potentiometers and im not a...

Marc3 by Associate III
  • 947 Views
  • 0 replies
  • 0 kudos

STM32H735 custom board power draw

Hi,Ive made a custom board with a STM32H735 micro on it. I have built a board with nothing but a micro and a few of its needed passive components and went to provide it power and test that its working. I supplied power from a benchtop power supply wi...

HAL_Delay blocks the entire program

Hello everyone. I have a big problem with my custom STM32H7 board, in particular with HAL_Delay.When I add a line on my main.c file to simply print on SWV, the first time seems to work, but after it does not work anymore. It prints the first time, an...

yaxsomo by Associate III
  • 3943 Views
  • 7 replies
  • 0 kudos