STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flashing chip on pcb

I am trying to flash a chip on a PCB. Right now I just have it toggle an LED. Sometimes it connects, but does not toggle, only stays lit. After power cycling, it does not even light up, it just stays off. Is there something i am missing, perhaps in t...

at3 by Associate III
  • 21122 Views
  • 18 replies
  • 8 kudos

Resolved! EEPROM SPI Reading issue

Hello, I am trying to write and read from stm32f105 to an eeprom 93AA46A, using Full-Duplex Master. To write into the eeprom, I am using following code:void EEPROM_WriteEnable(void) { uint8_t cmd = EEPROM_CMD_WRITE_ENABLE; //0x98 EEPROM_CS_H...

Siva21 by Associate II
  • 6740 Views
  • 17 replies
  • 5 kudos

Resolved! INTERFACING 32bit RAM With STM32H750XB MCU

Hi,     Please share pointers on interfacing 32Bits RAM along with STM32H750XB MCU with QUAD SPI External Memory and 8 MB Frame Buffer RAM on STM32H750XBRAM - IS42S32400TFT USED  - 1024x600 at 24 bpp and or 1024x800 at 16 bpp at 60 + FPSAre These Set...

32bit RAM.png
Caan by Senior
  • 2101 Views
  • 3 replies
  • 0 kudos

Low cost 16bit ADC

Posted on February 11, 2015 at 13:01Hi, Does anyone familer with Low cost microcontroller with 16bits ADC  (below 1.5$) ? Thanks

udibit by Associate II
  • 4608 Views
  • 6 replies
  • 0 kudos

Re: Tristating GPIO as an output

I used the code below but not working , did you find the solution ?   void SetPinTristate(GPIO_TypeDef *GPIOx, uint16_t GPIO_Pin) { GPIO_InitTypeDef GPIO_InitStruct = {0}; GPIO_InitStruct.Pin = GPIO_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; // Swi...

ramin110 by Associate II
  • 1530 Views
  • 3 replies
  • 0 kudos

STM32U5 option byte writting through bootloader

Hello, I am trying to write to the option byte area of an stm32u5g9vjt6q using the built in bootloader over the canFD protocol.  I have verified I am able to erase and write my programs to flash over canFD using the built in boot loader so I know tha...

brohr01 by Associate III
  • 1269 Views
  • 0 replies
  • 0 kudos

STM32F405 TIM DMA work only once

Hi ST team,I'm implementing DShot protocol with Timer + DMA. I use 4 PWM channels to generate control signals for ESC. Timer and DMA's parameters are same for all PWM channel. But PA3 (TIM2_CH4) does not work the same as other PWM channels. It only t...

phonght32_2-1740312861345.png phonght32_3-1740312876535.png Screenshot from 2025-02-23 19-06-36.png Screenshot from 2025-02-23 19-07-31.png

Unstable logical state on every I/O pin

Hi Everybody! I confronts a very interesting problem at my project. Details above:Hardware: NUCLEOG071RBAttached the IOC configuration. Control the SPI CS pin by software. I got small 4-8us signal spikes all  GPIO, SPI, I2S pins. SPI and I2S powered ...

pics2.png pics1.png
ProgBoy by Associate
  • 1692 Views
  • 2 replies
  • 0 kudos