STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RTC resets or stalls even with backup battery

I have an application running on STM32G491 which uses the RTC. There is an external 32768Hz crystal and a backup coin cell battery (I have checked that it is not depleted: 3.12V). There are two issues:Scenario #1: I pull the main battery, wait a bit,...

Resolved! Having Problems activating SysTick after Stop mode

I'm using STM32F070CBT at 8mhz with almost all pins active (used for GPIOs, PWM, SPI,I2C,etc) , i'm using a timer to enter stop mode with low power regulator and waking up using GPIO external event, after waking up i checked that PWMs and GPIOs are s...

HMucc.1 by Associate II
  • 3215 Views
  • 3 replies
  • 1 kudos