User Activity

Hi When I try to set DSI clock more than 500M, the STM32cubemx will display an error message "dsi clock source frequency must be =< 62MHz" as below. But it said STM32H747 DSI clcok can reach 1Ghz in datasheet.I use 25Mhz HSE and attach STM32cubemx pr...
Hi :Does anyone have en.stsw-link007_V2-33~en.stsw-link007_V2-35?For some reason, I need old stlink firmware.
Hi:When I try to download the latest stm32cubeide windows version from https://www.st.com/en/development-tools/stm32cubeide.html,I can only download a file which name is en.stm32cubemx-test-v20.zip. its URL ishttps://www.st.com/content/ccc/resource/t...
Hi I use STM32H743XI and W25Q256 for my design.And I notice W25Q256 has two speed 133Mhz(W25Q256JV) and 104Mhz(W25Q256FV), currently I use W25Q256FV, since I only use this flash with memory map mode, is it necessary to replace with W25Q256JV? Will th...
Hi:I use STM32L4P5RG with APS6404L-3SQR to develop GUI.I want use QSPI PSRAM as data memory for GUI.Now, I enable QSPI PSRAM as data memory as follows:1.configure QSPI PSRAM , SPI with NVIC in CubeMX2. add PSRAM (xrw) : ORIGIN = 0x70000000, LENGTH = ...
Kudos from
Kudos given to