STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is it possible to use Timer 3 in input capture mode on channel 1 and output compare mode on channel 3 simultaneously on STM32F103?

Posted on October 27, 2017 at 21:49Hello,I am using STM32CubeMX to configure the STM32F103C8T.  I want to use Timer 3 in two modes at the same time.  I want Timer 3 channel 1 in input capture direct mode and Timer 3 channel 3 in output compare chann...

pgregson1 by Associate III
  • 3057 Views
  • 6 replies
  • 0 kudos

Resolved! ADC with DMA with SW Trigger on L486 MCU

Posted on June 09, 2017 at 12:06I wish to use ADC1 to measure 6 channels and to have the results DMAd into memory.I am using CubeMX V4.21 and I think that I have set the parameters up correctly(See attached screen snip ADC_DMA_1 to 3.PNG)This sequen...

CubeMX 4.22.1 and SD card FatFs problem

Posted on October 25, 2017 at 15:45Hi, I'm currently trying to make SD card work with FatFS on a custom made PCB with STM32F429. I create the init files with CubeMX 4.22.1 and although I set the SD interface to be 4 bits long, I find this code in th...

Illogical EXTI code generation in CubeMX

Posted on November 01, 2017 at 10:50Hi all,I find the code generated by the CubeMX for EXTI line illogical.Every EXTI ISR (e.g. EXTI0_IRQHandler, EXTI1_IRQHandler calls for the same function: HAL_GPIO_EXTI_IRQHandler, which in turn also calls for th...

AC6 Firmware install fails

Posted on October 31, 2017 at 23:25Hi group,I have installed the AC6 Plugins in eclipse oxygen and try to create a test project for F3 Discovery.I've choosen Standard Peripheral Library and pressed 'Download Firmware'.There is something 32 MB downlo...

Ingo Wolf by Associate II
  • 1775 Views
  • 2 replies
  • 0 kudos

STM32F4 SDIO 4 bit mode with CubeMX project does not work

Posted on October 16, 2017 at 11:58Hi all,I created a project in CubeMX for a STM32F429IGtx with SDIO and FatFs. Clock at 180 MHz,The example works fine in 1 bit mode, but when I switch to 4 bit mode by adding the define 'BUS_4BITS'it does not work ...

Resolved! Trigger ADC Conversion with a Timer

Posted on October 12, 2017 at 22:25http://www.st.com/content/ccc/resource/technical/document/reference_manual/cf/10/a8/c4/29/fb/4c/42/DM00091010.pdf/files/DM00091010.pdf/jcr:content/translations/en.DM00091010.pdf talks about ADC external trigger and...

ee06091 by Associate III
  • 3372 Views
  • 4 replies
  • 0 kudos

Can't connect Nucleo 32 to USB

Posted on November 02, 2017 at 04:44 I’ve been through all the documentation and I’m getting very frustrated with this eval kit - it really shouldn’t be this difficult! Installed latest USB drivers, however the device is still not showing up unde...

Stcube header updates, but old problems.

Posted on November 01, 2017 at 12:54Hello,device headers of new release STM32Cube_FW_F2_V1.7.0 still have defines like#define GPIO_AFRH_AFSEL13_1 ((uint32_t)0x00200000U)I reported this misuse for uint32_t in the headers several time, with most other...