Resolved! MDF and ADC triggered from single EXTI
We want to trigger two conversions from the same EXTI (EXTI11).Basically rising edge on GPIO B11 should trigger ADC12 conversion and MDF (sigmadelta) Is it possible?
Ask questions, find answers, and share insights on STM32 products and their technical features.
We want to trigger two conversions from the same EXTI (EXTI11).Basically rising edge on GPIO B11 should trigger ADC12 conversion and MDF (sigmadelta) Is it possible?
Greetings Everybody, I am trying my hands with CAN FD. I have selected STM32C092RC for the same application as it has can fd port. I was wondering if MCP2561/62 can fd transiver ic works with this controller. Please advice. I was also looking for sch...
Hello everyone,I have three Nucleo 64 F401RE boards: two are used, owned by two of my friends, and they gave them to me, while one is new. The old boards have always worked fine, but the new one, which worked without issues for a while, no longer upl...
Hi everyone;I have select;In cube mx ->middleware and software packs -> CMSIS -> CMSIS Coremiddleware and software packs -> CMSIS - DSP middleware and software packs -> X Cube Algobuild -> DSP LibraryLater, I have select from software packs -> select...
Hello,I am making a project for myself on the STM32F405 control board KVM.This board receives data to the HOST from the mouse (this part works). Next, the MCU generates absolute coordinates. These coordinates (absolute) must be transmitted via USB to...
Controller: STM32H750XBH6 Development Environment: CubeMX + MDK V5.27Issue Background: The DAC chip requires the use of 32-bit SPI. Currently, it works normally with a polling method. There is a need to use hardware SPI + DMA to increase the speed.Wh...
The documentation mentions placing a ferrite bead between incoming voltage and the chip's VDDA line. Having limited knowledge of ferrite beads I'm confused as to which bead would work best. If the DC bias current should be about 20% of the bead's r...
I use cubemx generate a project with uart5. It's ok.But when I move some init codes of uart5 to function ``void SystemInit (void)`` tail as below```MPU_Config();HAL_Init();SystemClock_Config();PeriphCommonClock_Config();MX_UART5_Init();dbg_console_tx...
Hi there,We are working on a project in university. The objective of the project is to wirelessly transmit live camera feed to a LCD MIPI-4 Lane 50 pin screen using a digital camera module. We plan on using two microcontrollers, one for the camera wh...
Hello !Hope you're all doing well.I have a little problem here, my CAN BUS Tx is not working on "Normal Mode"I have a bus with several nodes communicating between them without any problem, so the bus itself is not the problemIn "Loopback mode" it wor...