User Activity

I have a structure that starts from my own bootloader, and I want to jump to the application. My question is similar to the one in this thread: Is it possible to keep dual bank active and executing the whole FLASH?  I am using the STM32G0B1RE microco...
Hello everyone,I’m facing an issue described in this link: My STM32 device is overheating and has malfunctioned.My STM32G070CBT MCU has been damaged, specifically from the PC6 pin, which wasn’t in use. Unfortunately, the pin is connected to another d...
Hello,We are planning to integrate the STSAFE110 into our device, which runs on Ubuntu. Since we’ll be developing our own code to retrieve the unique ID, I wanted to ask if there is any reference manual or documentation available for this. I couldn’t...
Hello,We’ve designed a device that uses an STM32 microcontroller to manage various features such as I2C, UART, ADC, IWDG, DMA, Flash memory handling etc. After running smoothly for a month, the device began malfunctioning, drawing 220 mA of current a...