STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC DMA TIM2 TRIGGER

Posted on March 25, 2018 at 12:29I want to use ADC which will be triggered by Timer 2 . I also want to use DMA to access adc converted data for fast sampling. Please help me for how to proceed?

STM32F7 - FMC SDRAM & NAND operation problem

Posted on March 26, 2018 at 09:11Hello ?My company is Korean distributor for Draupner Graphics, TouchGFX product.I am supporting ST Korea's TouchGFX users.I have technical issue regarding FMC SDRAM and NAND co-operation problem because SDRAM and NAN...

Resolved! stm32L496ZG dual boot

Posted on March 24, 2018 at 22:22hiim trying to implement dual boot using BFB2 bank switching on this chip, and after the code is burned in the second bank (ox80800000), it doesnt boot.i single stepped through the bootloader code, and it seems that ...

ron23 by Associate
  • 1111 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L071-RTC-SETTING

Posted on March 22, 2018 at 09:31hi all,   I'm using a board with one stm32l071.I have get code by stm32cubemx,and then I added my code on that.But now I have a issue with RTC,after I set the RTC registers, the hour in the register is less than my s...

0690X0000060A9mQAE.png
jz KN by Associate II
  • 1029 Views
  • 1 replies
  • 0 kudos

ECDSAsign

Posted on March 22, 2018 at 12:44Hi all,I am currently on a project which leverage the x-cube-cryptolib to send messages cross the network securely. To be specific, I want to use the ECDSA part to sign and verify my messages.  After some exploration...

STM32F4DIS-BB FatFs

Posted on July 14, 2017 at 20:24The original post was too long to process during our migration. Please click on the attachment to read the original post.

dbte by Associate II
  • 7127 Views
  • 21 replies
  • 0 kudos

TIM_ParallelSynchro on stm32f103xx not work

Posted on March 25, 2018 at 18:02I have implemented on stm32f103xx the example TIM_ParallelSynchro, this not work. For stm32f407xx fine work.int main(void){HAL_Init();SystemClock_Config();InitConfigTIM3_Master();InitConfigTIM2_Slave();while (1){}}st...

STM32L011D3 and L6387ED problem

Posted on March 24, 2018 at 12:39Hi,I'm using STM32L011D3 to control L6397ED driver. Everything works fine until supply voltage on L6387ED drops below threshold voltage (typ. 6V). When voltage drop on driver occurs, supply voltage on microcontroller...

Piotr1 by Associate II
  • 2636 Views
  • 6 replies
  • 0 kudos

Best way to configure clock [from scratch project]

Posted on March 24, 2018 at 17:51Hello everyone,I'm starting a blank project and would like to know the best way to configure the clocks (without using CubeMX).The initial project therefore contains the startup file stm32f413xx.s as well as the file...

Jems On by Associate III
  • 3692 Views
  • 7 replies
  • 0 kudos

STM32F0 bxCan Filters

Posted on March 24, 2018 at 22:40 Hello Today i was playing around with the bxCan module in a NUCLEO-F091RC, and trying to understand how the filter works. Afterrading some posts here in the forum i was able to understand the concept of ID ...