cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_SPI_Receive never returns by timeout

Santiago Alvarez
Associate
Posted on December 06, 2017 at 23:27

Hello everybody! I'm trying to implement some examples using the hal spi library in the B-L072Z-LRWAN1 (LoraWAN Discovery Board). This board has a STM32LO on it, and I'm trying to implement spi communication with an Arduino.

The ST LoraWAN discovery board is working as slave and Arduino as Master. 

Everything seems to work fine until I turn off the Arduino Board. When I do that, my program never returns from the following call:

status = HAL_SPI_Receive(&SpiHandle2, (uint8_t *)aRxBuffer, 2, 500);

Can't anybody point me in the right direction to discover what I'm doing wrong?

Thanks!

#stm32lo #spi #timeout
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0