cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 I2C problem with comunnication

Jan Nowak
Associate
Posted on December 06, 2017 at 18:27

Hello. I configured stm32 PB11 and PB10 as SDA and SCL pins then i connected GY-30 BH1750 light sensor.

It's address is 0x23 when ADDR pin connected  to GND.

POWER_ON 0x01

RESET 0x07

BH1750_CONTINUOUS_HIGH_RES_MODE 0x10

This is function to send the data: 

void WriteBuffer(uint8_t I2C_ADDRESS, uint8_t *aTxBuffer, uint8_t TXBUFFERSIZE){

failure=0;

   while(HAL_I2C_Master_Transmit(&hi2c2, (uint16_t)I2C_ADDRESS<<1, (uint8_t*)aTxBuffer,          (uint16_t)TXBUFFERSIZE, (uint32_t)1000)!= HAL_OK)

         {

failure =1 ;

if (HAL_I2C_GetError(&hi2c2) != HAL_I2C_ERROR_AF)

{

Error_Handler();

}

}

   while (HAL_I2C_GetState(&hi2c2) != HAL_I2C_STATE_READY)

   {

   }

}

uint8_t buffer[3];

buffer[0] = POWER_ON

and when i call WriteBuffer(0x23, buffer, 1), function return 1 in failure variable and data isn't sent.

I check variables in STM Studio. Where can be problem? Is this code fail or my connections between sensor and STM ?

#i2c-sensor
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0