STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 OV7670 DCMI

Hello, for a few days I have been trying to run the OV7670 camera on the STM32F446RE (Nucleo).Since the full QVGA RGB565 (153600 B) does not fit in RAM, for now i opted for QVGA Y8 Grayscale, however i must have some problem with how im configuring s...

Open ocd SWD Programming with CMSIS-DAP

Hi everyone,iIm currently trying to program an STM32F0x MCU with an CMSIS-DAP interface on openocd, but i'm currently able to generate only an useless reset signal :In Yellow the SDIO and in Purple the RSTSo when i'm trying to generate this reset sig...

Quentin_27_0-1741856714617.png

help with spi setup with rc522 module

Posted on February 05, 2014 at 17:35Hi-I'm quite new to stm32 and emededded development so please bear with me.I've purchased a Sain Smart RC522 RFID reader/writer (https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&ved=0CDwQFjA...

gecono by Associate
  • 13259 Views
  • 16 replies
  • 0 kudos

Resolved! VREF+ on the STM32H743VIT6

Hello,This is the first time I'm working with an STM32 and I have a question regarding the VREF+ pin. I'm creating a schematic for the MCU and I'm not entirely sure what to do with the VREF+ pin and I'd like some clarification on something. According...

felron124 by Associate II
  • 3272 Views
  • 7 replies
  • 2 kudos

DMA DAC STM32F405RGT6 underrun

We have STM32F405RGT6 and we want to implement DAC through DMA.We used an example for STM32F429ZI-NucleoHere is an actual code where we have an underrun the error and we need help to clarify reason and find a solution, thanks!:   #include "main.h" #i...

Godzilla by Associate
  • 1153 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 with built in flash?

Hi,Does anyone know if there is a chance for a new N6-device later this year having built in flash of at least 4MB?Our project is currently based on a one chip solution with a custom U5-board with built in FLASH/RAM of 4MB and a 5” Riverdi display. H...

Resolved! USB HS Device fails to bring up if ETH is activated

Hi,I am using an STM32H7RS MCU (NUCLEO-H7S3L8) and I need to use both USB HS Device and Ethernet MAC.For Ethernet MAC I will only need to use MDIO interface, so I don't think I need a stack for it but please correct me if I am wrong.The MX_ETH_Init c...

simo zz by Senior II
  • 2059 Views
  • 3 replies
  • 5 kudos

I2C slave with no clock stretch

Posted on October 23, 2017 at 12:33Hello,I've tried the I2C_TwoBoard_RestartComIT example in the STM32Cube_FW_L4_V1.9.0. It works fine.If I disable the clock stretching feature, the slave can still receive messages, but it doesn't transmit back. It ...

Resolved! STM32 Nucleo-F401re bootloader commands are not working

usart1 connectedHercules setup utility     Issue with Sending Bootloader Command on STM32According to AN3155, the 0x7F command should initialize the USART. I have ensured that I am in bootloader mode and have made the following connections:Connect th...

mohite25_0-1738652856579.png mohite25_1-1738653591496.png
mohite25 by Associate III
  • 1340 Views
  • 1 replies
  • 0 kudos