STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

why I can not use LPUART?

I want to communicate with a UART module using an STM32H723 Nucleo board. Receiving data and transmitting over DMA features. İf i choice USART2: PD5 (TX) and PD6 (RX) it works fine? İn same code if change usart2 to lpuart and if i change pins for lpu...

fixaj by Associate II
  • 1420 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 with LQFP package?

New question moved from this thread.Hi again, A related follow-up question: Any plans of a N6-version in a LQFP-package this year? Thanks in advance

HAL_SPI_TransmitReceive problems

I am having problems trying to use the HAL_SPI_TransmitReceive function. I am using STM32CubeIDE along with the STM32U5G9J-DK2, I am configuring my side as a full duplex slave using the following parameters:I am working with an embedded processor tha...

Ron54_1-1741900491831.png Ron54_2-1741900774954.png Ron54_3-1741902302260.png
Ron54 by Associate
  • 1349 Views
  • 1 replies
  • 0 kudos

STM32H7 ADC clock prescaler

HelloI'm always confused with the ADC clock config of H7 devices. ok, H7 is not a device for noob but ever after spending days reading datasheets, users manual, appnote, and filling spreadsheets, when starting cube MX, you will always find that the c...

clock cfg.png
tarzan2 by Senior
  • 1239 Views
  • 1 replies
  • 0 kudos

STM32F413CGU6: Reset after Erase Memory command via I2C

Hello,with an ESP8266 I execute an erase memory command for the STM32F413CGU6 and when the sector is erased, the STM32 always performs a reset. The sector is erased afterwards, but the ESP doesn't have acces to the Boot0 pin and afterwards the STM32 ...

Eric_Z by Associate II
  • 1259 Views
  • 3 replies
  • 0 kudos

Resolved! External DAC SPI interface speed optimization

Hi,I'm using the NUCLEO-H743ZI2 board and I'm trying to interface it with an external DAC MCP4922 via SPI.As explained in the documentation, the CS pin is very important because it is used to mark the end of a transmission for the DAC to put the rece...

jmF_0-1741702725267.png jmF_1-1741788222878.png jmF_2-1741788257304.png jmF_3-1741788660744.png
jmF by Associate II
  • 2179 Views
  • 4 replies
  • 1 kudos

Resolved! Stm32f446re CAN start error

  CAN Bus Not Starting - HAL_CAN_Start() Error (0x00020000) Post: I'm facing an issue where my CAN bus does not start. Tera Term shows the following messages:   less CopyEdit CAN1 Instance Address: 0x40006400 CAN Error Code: 0x00020000   Co...

Yakry by Associate II
  • 965 Views
  • 1 replies
  • 0 kudos

PWM Deadtime

I need to generate deadtime of top and bottom PWM CH1 and CH1N about 1.5us. I set deadtime 190 and it has 1.5us deadtime, but I dont understand... I need you :loudly_crying_face:  

GIABAO_0-1741852495230.png
GIABAO by Associate
  • 949 Views
  • 2 replies
  • 0 kudos